Hello Bernie,
Thanks for the reply,
I had one more question, about the Uboot and Emac bootloaders.
I found a couple of posts using EMAC Bootloaders.
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/439/p/11468/44656.aspx#44656
http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/112/p/11469/44671.aspx#44671
They both are using EVM6486 chips and EMAC booting, both also mention Uboot. Is the EVM6486 similar to EVM6472 since, they are the same architecture??
Can we use, UBOOT to boot the EVM 6472 board?? If UBoot boots the EVM6486 board what OS is it using and can it be replicated on EVM 6472?
If yes, does TI have any documentation to support this? Do you think we should pursue with the U-boot approach as boot loader or use the native TI boot loader that came with EVM6472?
Please