This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

use coprocessor for image processing functions



Hi

I use DM6467T it has two coprocessor

is there any library and function  to  scaling and a fine transformation  by coprocessor?

  • Hi,

    Thanks for your post.

    In general, the scaling is to be done on the DSP or using the Hardware accelerators. The downsizing is available as the VDCE driver and it is totally dependent on ARM cycles. This is on DM6467T. Both upsizing and downsizing can be implemented using the DSP C64x based algorithms. However any resolution more than 1080p will have the limitation on the DSP cycles. Other platforms like DM365, DM6446 and DM6437 have both upsizing and down sizing possible on hardware.

    The H.264 compression is done by the HW accelerator on DM6467 and the resizing has to be done by the VDCE or DSP once the frame is decoded by the accelerator on the DM6467T.

    The video analytics available as part of DM6467 will work the same way as on DM6467T. The DVSDK will include the Video compression software, PSP releases and demos. Check the DVSDK contents.

    For more info. kindly refer the below links:

    http://www.dm6467t.com/evm/#dm6467tevmspecifications-1

    http://www.dm6467t.com/files/DM6467-EVM-TI-DaVinci-High-Definition-Evaluation-Module.pdf

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------

  • thanks
    I see there is a vico library for dm6446 is there any library for dm6467t
    coprocessor in dm6467 use for compression?