Hi, we've got a custom board with an OMAP L138 powered by a TPS65023. We followed the example design for the TPS portion from SLVA340.
In general it works. But, if the board has been turned off for a few minutes before power is applied, there's a really good chance that the DSP will not communicate with the ARM. The ARM works and boots as normal, but once we get to the DSPlink, the ARM applicaiton hangs.
When the problem occurs we see that the board draws about 100mA more current than it should on power up. If we see this power condition, you are 100% guarateed to have an unresponsive DSP. If I power cycle the board a couple of time I can get it to the point where the current is normal and everything works fine.
I'm guessing that it has something to do with the power-up sequence, or a noisy supply. We are following the connections from SLVA340 strictly, so I think the power-up sequence is correct.
Has anyone else seen this issue.
Thanks,
John Fielden