Other Parts Discussed in Thread: TMS320DM6467T
Hi,
Please suggest me good processor for 3d image processing (adaptive filtering ) and camera support application.
Thanks in advance,
Ravishankarkm
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320DM6467T
Hi,
Please suggest me good processor for 3d image processing (adaptive filtering ) and camera support application.
Thanks in advance,
Ravishankarkm
Hi,
Thanks for your post.
In my understanding, TMS320DM6467T, a new DaVinci video processor designed to meet the demand for increased digital video quality, higher resolution and faster frame rates for video communications and security applications. The 1 GHz DM6467T is a single-chip processor that enables networked digital video applications to decode high-definition (HD) H.264 (1080p at 60 frames per second (fps)).
Key features:
The combined performance of a 1 GHz C64x+(TM) DSP and 500 MHz
ARM926EJ-S
-- Supports H.264 1080p decoding up to 60 fps, a well as eight
simultaneous channels of H.264 D1 real-time video encoding with
solution from a third party
-- Higher core speed with flexible DSP programmability provides
sufficient processing capacity to implement advanced video processing
algorithms and functions
-- Faster DDR2 interface at 400 MHz facilitates higher bandwidth for more efficient video throughput
-- Two integrated 500 MHz High Definition Video/Imaging Co-Processors
(HD-VICP) accelerate video processing and increase application
efficiency
-- Faster 150 MHz video port interface supports 1080p capture
For more info. kindly refer the below links:
http://www.dm6467t.com/evm/#dm6467tevmspecifications-1
http://www.dm6467t.com/files/DM6467-EVM-TI-DaVinci-High-Definition-Evaluation-Module.pdf
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question
-------------------------------------------------------------------------------------------------------