Other Parts Discussed in Thread: SYSBIOS
Hi,
Long story short, we need the bios libraries built without the -g option so that the .out files (and resulting xml files from the ofd6x.exe tool) are not so large. We need to extract information about the global symbols and types from the xml file and only care about global symbols and types that "our part of the code" declares/defines.
Is there such a build available? If not, is there a CCS project for the BIOS library that will let us build it with the options we desire?
Will it link ok with our code, which is built with the -g option?
CCS V4.
Bios: V6_21_00_13
Thanks for your help,
Shawn