Other Parts Discussed in Thread: AM5728
Hello,
I'd like to build SBL for AM5728 Processor SDK RTOS v2.0.2.11 (PDK v1.0.2) on Windows. I see error messages during building sbl.
--------------
C:\ti\pdk_am57xx_1_0_2\packages>pdksetupenv.bat
Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
SUPPORTED_PLATFORMS : "am571x am572x"
PDK_INSTALL_PATH : /ti/PDK_AM~2/packages/
C6X_GEN_INSTALL_PATH : C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0
TOOLCHAIN_PATH_A15 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8
-2014q3
TOOLCHAIN_PATH_A8 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8
-2014q3
TOOLCHAIN_PATH_A9 : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8
-2014q3
TOOLCHAIN_PATH_M4 : C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.5
FPULIB_PATH : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8
-2014q3/lib/gcc/arm-none-eabi/4.8.4/fpu
CROSS_TOOL_PRFX : arm-none-eabi-
XDC_INSTALL_PATH : C:/ti/xdctools_3_32_00_06_core
BIOS_INSTALL_PATH : C:/ti/bios_6_45_01_29
IPC_INSTALL_PATH : C:/ti/ipc_3_42_00_02
EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_2_12_01_23
NDK_INSTALL_PATH : C:/ti/ndk_2_24_03_35
IMGLIB_INSTALL_PATH : C:/ti/imglib_c66x_3_1_1_0
UIA_INSTALL_PATH : C:/ti/uia_2_00_03_43
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: /ti/PDK_AM~2/packages/
PDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
C:\ti\PDK_AM~2\packages>cd ti/boot/sbl
C:\ti\PDK_AM~2\packages\ti\boot\sbl>gmake example BOARD=evmAM572x SOC=AM572x
gmake[1]: Entering directory `C:/ti/PDK_AM~2/packages/ti/boot/sbl'
linking /ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/armv7/obj/sb
l_multicore_mpu.o /ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/ar
mv7/obj/mailbox.o /ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/ar
mv7/obj/UART_soc.o into /ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/exam
ple/armv7/bin/sbl_app.out ...
/ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/armv7/obj/sbl_init.a
o: In function `IRQHandler':
/ti/PDK_AM~2/packages//ti/boot/sbl/soc/am57xx/sbl_init.S:211: undefined referenc
e to `INTCCommonIntrHandler'
/ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/armv7/obj/sbl_init.a
o: In function `UndefInstHandler':
/ti/PDK_AM~2/packages//ti/boot/sbl/soc/am57xx/sbl_init.S:169: undefined referenc
e to `start_boot'
collect2.exe: error: ld returned 1 exit status
gmake[1]: *** [/ti/PDK_AM~2/packages//ti/boot/sbl/binary/evmAM572x/example/armv7
/bin/sbl_app.out] Error 1
gmake[1]: Leaving directory `C:/ti/PDK_AM~2/packages/ti/boot/sbl'
gmake: *** [example] Error 2
C:\ti\PDK_AM~2\packages\ti\boot\sbl>
--------------
It looks like the errors are caused by the following makefile. So I add sbl_startup.c for undefined Handlers to the makefile. The errors are solved, but another errors occur. Please give me advice.
C:\ti\pdk_am57xx_1_0_2\packages\ti\boot\sbl\example\mpuMulticoreApp\makefile
Regards,
Kazu