hi,
1. I am using TMS320C5515 EVM with ADS1298R and trying to run the demo code: ADS1298_ECGSystem_C5515EVM. In the past I succeeded to get the desirable lcd screen (after changing JP24 to supply 3.3V instead of 1.8V), but now the code stuck at infinite loop. after debugging I noticed that SPI initialization failed at the spi driver configuration (at DDA_spiConfiguration routine) .In the code it failed because the values of spiCtrlMode (0xFFFF) didn't match to SPI_MODE (0) (the spiMaster didn't match too and so opMode and etc). I don't succeed to run it as before. any advice?
2. In the past, when the demo code run succeesfuly, I tried to use the C55x ECG ADS1298 Medical Development Kit (MDK) application but I got error (in the bottom of the gui): SERIAL PORT DISCONNECTED (although the serial port was connected with the requested baud rate: 115200)
3. another issue is about baud rate: while running CSL_UART_INTEXAMPLE I got NULL at the terminal when the baud rate was as requested (2400). after testing it in lots of rates - it worked at baud rate 352. It's very low. isn't it? what I should change to get the normal rate?
hope someone could help me,
thanks in advance!!
Keren