This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eQEP dropped in OMAP-L138

Other Parts Discussed in Thread: OMAP-L138, OMAP-L137

I am investigating upgrading a design in progress from an OMAP-L137 to an OMAP-L138.

 

I noticed that the two 32 bit Enhanced Quadrature Encoder functions present in the OMAP-L137 are not in the OMAP-L138.  Why was this omitted in the L138?  Is there another function that could be used to capture encoder inputs, like eCAP etc.  Or was it a marketing decision based on its potential use?

When I generated the comparison spreadsheet between the OMAP-L137 and OMAP-L138 a column was not generated for the eQEP.  I found that the eQEP was not present by looking at the block diagrams for the two parts.  Why was this omitted from the spreadsheet?  This appears to be the only feature dropped going from the L137 to the L138.

 

  • There are some trade-offs between the OMAP-L137 and OMAP-L138. 

    For instance, OMAP-L137 has 2 eQEPs and 3 ePWMs.  OMAP-L138 doesn't have eQEPs and only 2 ePWMS, but it does have a new set of peripherals, such as McBSP, uPP, SATA, VPIF, DDR, etc.

    Therefore, your device selection should depend on your application requirements.

    - Christina

  • One of OP's questions wasn't answered:  "Is there another function that could be used to capture encoder inputs? "

    I need a direct interface with a rotary incremental encoder to get position, direction & speed information.  What are solutions (HW or SW) since my OMAP-L138 system doesn't have eQEP?