This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDC tool error when implement SYS/BIOS+StartWare on ARM of OMAPL138

Other Parts Discussed in Thread: OMAPL138, SYSBIOS

Dear all,

I am trying to implement SYS/BIOS  on ARM of OMAPL138, and include lib of startware for omap.

I use : 

- sys/bios 6.45.1.29

-startware 1.10.04.1

-xdc tool 3.31.3.41

I create a typical example project with sys/bios on arm of omap, and include lib of startware:

"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\cgt_ccs\omapl138\lcdkOMAPL138\platform\Debug\platform.lib"
"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\cgt_ccs\omapl138\system_config\Debug\system_config.lib"
"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\cgt_ccs\utils\Debug\utils.lib"
"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\cgt_ccs\omapl138\drivers\Debug\drivers.lib"
"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\gcc\omapl138\drivers\Release\libdrivers.a"
"C:\ti\OMAPL138_StarterWare_1_10_04_01\binary\armv5\gcc\omapl138\lcdkOMAPL138\platform\Release\libplatform.a"

follow the gpio example of Startware, i wrote init GPIO and toggle led, build success, then when i run debug with omapL138LCDK kit, in console window:

[ARM9_0] size: 0x2000.
R0 = 0x01e27000 R8 = 0x80000020
R1 = 0x00000003 R9 = 0x000000cd
R2 = 0x00000283 R10 = 0x24d288de
R3 = 0x00000001 R11 = 0x88bec058
R4 = 0xffff0700 R12 = 0x00000003
R5 = 0x00000000 SP(R13) = 0x80000020
R6 = 0xc300adb8 LR(R14) = 0xc300ae94
R7 = 0xc300ae94 PC(R15) = 0x80000020
PSR = 0xc300adb8
DFSR = 0x00000005 IFSR = 0x00000008
DFAR = 0x01e27a0c
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x80000020, lr = 0xc300ae94.
xdc.runtime.Error.raise: terminating execution

Anyone can tell me what happen and the solution? 

Thanks you so much.

Regards,

Nhan