This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 minicom baudrate

Dear sir,

Am new to this board and booting from sd card by setting up the sw3 and sw4 settings,but we are not getting any thing in minicom,we checked for 9600 and 115200,but we dint get.what shpuld be the baud rate.we are getting green back ground in hdmi connection ,here in manual it is given black background.is it ok?

And we wanna do ome image processing on this board.Can we get standard demos from texas?please send me the standard demos.

If you have any type of standard demos ,please share the link.

thank you

  • Hi Mohammad,

    The baud rate is 115200. Refer to the below pointers for more info on how to config the console:

    ti-ezsdk_dm816x-evm_5_05_02_00/docs/DM816x_EZ_Software_Developers_Guide.pdf - 6.6 Setting up Tera Term
    processors.wiki.ti.com/.../Setting_up_Minicom_in_Ubuntu
    processors.wiki.ti.com/.../TI81XX_PSP_User_Guide
    processors.wiki.ti.com/.../TI81XX_PSP_UBOOT_User_Guide
    processors.wiki.ti.com/.../TI81xx_PSP_Porting_Guide

    The standard demos are available into the EZSDK package.

    Regards,
    Pavel
  • Thank you pavel,
    I need the the EZSDK Package Link,which one i need to download.
    can we work on ubuntu 14?
  • The link to the latest (5.05.02.00) EZSDK:
    software-dl.ti.com/.../index_FDS.html

    It is tested under Ubuntu10,11,12 but it might work on Ubuntu 14 also (it is not tested). You need to modify the below script for Ubuntu14:

    ti-ezsdk_dm816x-evm_5_05_02_00/bin/setup-host-check.sh

    BR
    Pavel
  • Thank you pavel,

    In other kits like Devkit or Beagle bone,after booting from sd card,there will be a image given by respected companies,if we just copy into the sd card and run it ,it will show the output,

    like this,can we do with this board means the copying of standard images to the sd card and just running it by minicom..?

    where i ll get the standard codes .?We purchase the kit ,with that two cd's came one is for ubuntu and other is for code sourcery,is code sourcery contains standard images?

    my last doubt is that,can we purchase a sd card from outside and copy the images from the sd card what texas has given with the kit,and can we run the board using new sd card..?is the images of sd card read only..?

    thank you

  • Mohammad,

    MOHAMMAD NASEER M N said:

    In other kits like Devkit or Beagle bone,after booting from sd card,there will be a image given by respected companies,if we just copy into the sd card and run it ,it will show the output,

    like this,can we do with this board means the copying of standard images to the sd card and just running it by minicom..?

    Yes, there are pre-built images (MLO, u-boot.bin, uImage) that you can place in your SD card and boot the DM816x TI EVM from that SD card. These images are located in ti-ezsdk_dm816x-evm_5_05_02_00/board-support/prebuilt-images/

    MOHAMMAD NASEER M N said:
    where i ll get the standard codes .?We purchase the kit ,with that two cd's came one is for ubuntu and other is for code sourcery,is code sourcery contains standard images?

    Usually the DM816x TI EVM come with one SD card, with pre-built images on it. But these images might be not from the latest EZSDK version (5.05.02.00) but from older release of the EZSDK. Thus I would recommend you to run the setup script, which prepare the SD card for you with the latest images, see the below doc for more info:

    ti-ezsdk_dm816x-evm_5_05_02_00/docs/DM816x_EZ_Software_Developers_Guide.pdf
    6.7 How to create an SD card

    MOHAMMAD NASEER M N said:
    my last doubt is that,can we purchase a sd card from outside and copy the images from the sd card what texas has given with the kit,and can we run the board using new sd card..?

    Yes, you can get your own SD card and use it.

    See also if the below e2e thread will be in help:

    Regards,
    Pavel

  • thank you pavel,i got lot of information from you.
    please close this thread,if i get any doubt i ll creat a new thread.