This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query about use of C6713 DSK in applications related to image processing



 

Hi Mukul and JohnS,

Thanks for your reply.

i wrote the below:

Hi Everyone,

I just want to know that can  TMS320C6713DSK be used for image processing applications like reading and loading an image?

And if yes, please let me know that how we can do this?

There is one more problem i am facing that can we use TMS320C6713DSK with CCS4.1?

Actually Mukul i am an intern in TI itself, i am working on a project which is based on "image encryption using fractional fourier transform". i just want to know that what processors or microcontrollers will be useful for my project.

  • Gauri,

    Although this question is probably better answered in the C67 processor forums, I give below some inputs that could help your project.

    - The C6713 can be used for image processing applications, however its suitability to a specific application is heavily dependent on the image characteristics (size, color depth, etc.) and the type of processing required (real-time or post-processing). Its speed should be fine to process static images or low-resolution video (CIF, VGA), however don't expect it to handle HD video streams.

    - Differently than the DM counterparts, both the C6713 and its DSK do not have video ports, therefore any image capture device would require external hardware;

    - The C6713DSK can be used with CCSv4.1 without problems. Just follow the instructions to configure the target at the page below:

    http://processors.wiki.ti.com/index.php/GSG:Common_target_configurations

    I will move this thread to the C67x processor forum. There you may be able to get additional help about the application.

    Hope this helps,

    Rafael