This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Graphics SDK Install Issue!

Hi,

I can build the graphics sdk successfully. AFter that I write make install but get an error. Error is it cannot find modules.order. I checked the linux source dir and there is no such file. How can I create that file or solve my issue?

My Graphics SDK: 3.01.00.06

DVSDK: 3.01.00.03

PSP-SDK: 3.00.00.05

Thanks.