This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6746]Can same power supply be used for static 1.8V IO supplies and LVCMOS IO supply groups?

Dear Champs,

Could you please let me know if same power supply can be used for All static 1.8V IO supplies(DVDD18, DDR_DVDD1.8, and USB0_VDD1.8) and all of the LVCMOS IO supply groups used at 1.8V nominal(DVDD3318_A, DVDD3318_B, and DVDD3318_C)?

in below schematic, I would like to check if CVDD18 and DVDD18 can be combined into same power supply.

Thanks and Best Regards,

SI.