Hi,
May the following register of AM335x change setting dynamically?
①System (Transfer Controller) Priority
9.3.1.16 init_priority_0 Register (offset = 608h)
9.3.1.17 init_priority_1 Register (offset = 60Ch)
9.3.1.31 mreqprio_0 Register (offset = 670h)
②LCDC dma priority
13.5.1.16 dma_master_prio bit of LCDDMA_CTRL Register
③EDMA
TC priority
11.4.1.8 QUEPRI Register
DBS
9.3.1.18 tptc_cfg Register (offset = 614h)
④EMIF
7.3.5.15 REG_PR_OLD_COUNT bit field of OCP_CONFIG Register
When those setting dynamically is it in a problem, please tell me which timing those registers should set it in.
Best Regards,
Shigehiro Tsuda