All,
How do I test my SPI1 interface?
I decided to buy the MSP-EXP430F5438 experimenter board which is close to what we are using.
I am a complete noob to TI DSP and now MSP.
Software: Is there SPI1 example code available to send small data between on the TMS320C6748 and MSP-EXP430F5438?
(need example for MSP as well as 6748).
Hardware: What do I need to do to physically connect SPI1 between the two eval boards?
Any help would be greatly appreciated.
Thank you in advance.