This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168 video examples error

Dear sir,

I was trying the standard examples given by texas in ez in the path usr/local/ez/example-application/linux driver..../video.

in this i was able to run only one program which was showing the details of screen and when i try for rest of the programs there,by doing "gcc examplename.c" am getting error.

why am getting error..?is the code given by texas is not completed one..?do we need to add any thing in the code..?how to solve this problem..?

then am having a small doubt that this standard programs  usr/local/ez/example-application/linux driver..../video.,i need to run it in MINICOM or in terminal window?

i think by minicom,because by minicom only i am connected to the board..am i right..?

  • Hi Mohammad,

    MOHAMMAD NASEER M N said:
    I was trying the standard examples given by texas in ez in the path usr/local/ez/example-application/linux driver..../video.

    Do you mean the below path?

    ti-ezsdk_dm816x-evm_5_05_02_00/example-applications/linux-driver-examples-psp04.04.00.01/video

    If yes, then refer to the below files/links for how to run these video demos:

    ti-ezsdk_dm816x-evm_5_05_02_00/example-applications/linux-driver-examples-psp04.04.00.01/video/bin/ReadMe

    Regards,
    Pavel