Other Parts Discussed in Thread: DM3730, TPS65920
Hello. I have developed DM3730 based custom board. It have TPS65920 PMIC with 26MHz oscillator. I have managed to boot this board and it works fine (except for bad TPS65920 starting), but console baud rate is 76800. It is a problem for linux terminals. I also have devboard with DM3730, TPS65920 and 26MHz oscillator, and it boots at 115200 baud rate. Linux image is the same.
Does DM3730 has ROM configuration?