I'm running a C6455 (with MACSEL configured for GMII) on a custom board . I can't get the TI DSP to talk to the PHY. Looking at the MACSTATUS register, IDLE (bit 31) is 0. In the EMAC/MDIO documentation (spru975b pp115) it states:
"EMAC idle bit. This bit is set to 0 at reset; one clock after reset it goes to 1.
0 The EMAC is not idle
1 The EMAC is in the idle state"
Which clock is this referring to?