This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

S-Video output testing in DM8168

Hi,

We are testing S-Video output from DM8168.

To test this, We executed display application found in TI OMX demo, the system hangs during execution.

Below are the Log captured

/usr/share/ti/ti-omx# ./display_a8host_debug.xv5T -d 2
display_id: 2
Display example
===============================
 OMX_Init completed
 UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
found handle 0x12f018 for component OMX.TI.VPSSM3.VFDC
 got display handle
found handle 0x135828 for component OMX.TI.VPSSM3.CTRL.DC
Buffer Size computed: 518400
set input port params (width = 720, height = 480)
setting input and output memory type to default
enable input port
got eventEnable/Disable Event

Please suggest us what could be the reason for the hang or suggest us the steps to test s-video output from DM8168.

Regards,

Geetha

  • Hello,

    What is the Ezsdk version that you are using here?
    What you are using custom board or evm?

    BR
    Margarita
  • Hi,


    We are using ti-ezsdk_dm816x-evm_5_05_02_00 version and custom board.


    .

  • Hello,

    Could you attach the full debug log ?

    For getting more debug prints run ./loggerSMDump.out 0x9e400000 0x100000 all

    This is available at /usr/share/ti/ti-uia folder in filesystem.

    BR
    Margarita

  • Hi Margarita,

    Below are the complete log for the issue obtained by executing

    ./loggerSMDump.out 0x9e400000 0x100000 all

    /usr/share/ti/ti-omx# ./display_a8host_debug.xv5T -d 2
    display_id: 2
    Display example
    ===============================
     OMX_Init completed
     UIAClient is ready to send a UIA configuration command
    UIAClient received UIA_CONFIGURE_ACK
    UIAClient is done sending requests
    UIAClient is ready to send a UIA configuration command
    UIAClient received UIA_CONFIGURE_ACK
    UIAClient is done sending requests
    N:Video P:1 #:00031 T:00000275a188d8c9 M:xdc.runtime.Main S:Enabling Status Logger
    N:VPSS  P:2 #:00033 T:00000275a175f993 M:xdc.runtime.Main S:Enabling Status Logger
    N:Video P:1 #:00032 T:00000275a1894897 M:xdc.runtime.Main S:Enabling User1 Logs
    N:VPSS  P:2 #:00034 T:00000275a1766c41 M:xdc.runtime.Main S:Enabling User1 Logs
    N:Video P:1 #:00033 T:00000275a189c58f M:xdc.runtime.Main S:Disabling User1 Logs
    N:VPSS  P:2 #:00035 T:00000275a176d84f M:xdc.runtime.Main S:Disabling User1 Logs
    N:Video P:1 #:00034 T:00000275a18a2c53 M:xdc.runtime.Main S:Disabling User1 Logs
    N:VPSS  P:2 #:00036 T:00000275a1773573 M:xdc.runtime.Main S:Disabling User1 Logs
    N:Video P:1 #:00035 T:00000275a18a909b M:xdc.runtime.Main S:Disabling User1 Logs
    N:VPSS  P:2 #:00037 T:00000275a1779455 M:xdc.runtime.Main S:Disabling User1 Logs
    N:Video P:1 #:00036 T:00000275a18af75d M:xdc.runtime.Main S:Disabling User1 Logs
    N:VPSS  P:2 #:00038 T:00000275a177f345 M:xdc.runtime.Main S:Disabling User1 Logs
    N:Video P:1 #:00037 T:00000275a18b5fa3 M:xdc.runtime.Main S:Disabling Analysis Logs
    N:VPSS  P:2 #:00039 T:00000275a17857ab M:xdc.runtime.Main S:Disabling Analysis Logs
    N:VPSS  P:2 #:00040 T:00000275a1c5aa6f M:xdc.runtime.Main S:OmxRpc_rcmIfGetHandle:ComponentName:OMX.TI.VPSSM3.VFDC
    N:VPSS  P:2 #:00041 T:00000275a1c66f1f M:xdc.runtime.Main S:Entered function:omxrpc_module_init_client (3)
    N:VPSS  P:2 #:00042 T:00000275a1c714b5 M:xdc.runtime.Main S:Entered function:OmxRpc_rcmClientCreate (0x9f1debfc, OmxRpcRcmServer_3, 5)
    N:VPSS  P:2 #:00043 T:00000275a1c789a5 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_ini>
    N:VPSS  P:2 #:00044 T:00000275a1c8007f M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init>
    N:VPSS  P:2 #:00045 T:00000275a1c874db M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create>
    N:VPSS  P:2 #:00046 T:00000275a1cd5549 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create>
    N:VPSS  P:2 #:00047 T:00000275a1cde285 M:xdc.runtime.Main S:omxrpc_module_init_client: Located the remoteCoreRcmServer
    N:VPSS  P:2 #:00048 T:00000275a1ce5485 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcGetHandle)
    N:VPSS  P:2 #:00049 T:00000275a1d17555 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcFreeHandle)
    N:VPSS  P:2 #:00050 T:00000275a1d3f203 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCreateProxyLite)
    N:VPSS  P:2 #:00051 T:00000275a1d65ef5 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcGetHeapMemStats)
    N:VPSS  P:2 #:00052 T:00000275a1d8e185 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcDeleteProxyLite)
    N:VPSS  P:2 #:00053 T:00000275a1db4157 M:xdc.runtime.Main S:LayerId: 2
    N:VPSS  P:2 #:00054 T:00000275a1dbf1ad M:xdc.runtime.Main S:@ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_24
    N:VPSS  P:2 #:00055 T:00000275a1dc7415 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_i>
    N:VPSS  P:2 #:00056 T:00000275a1dceaf1 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_in>
    N:VPSS  P:2 #:00057 T:00000275a1dd5cbf M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create>
    N:VPSS  P:2 #:00058 T:00000275a1e387e1 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create>
    N:VPSS  P:2 #:00059 T:00000275a1e4158b M:xdc.runtime.Main S:@ omxrpc_rcm_server_remote_fxn_register regFxnCategory 1
    N:VPSS  P:2 #:00060 T:00000275a1e47b7d M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSetParameter)
    N:VPSS  P:2 #:00061 T:00000275a1e5177d M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetParameter)
    N:VPSS  P:2 #:00062 T:00000275a1e58d65 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSetConfig)
    N:VPSS  P:2 #:00063 T:00000275a1e5ff2b M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetConfig)
    N:VPSS  P:2 #:00064 T:00000275a1e66cbd M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetComponentVersion)
    N:VPSS  P:2 #:00065 T:00000275a1e6e74b M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetExtensionIndex)
    N:VPSS  P:2 #:00066 T:00000275a1e75c45 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetState)
    N:VPSS  P:2 #:00067 T:00000275a1e7fe55 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSendCommand)
    N:VPSS  P:2 #:00068 T:00000275a1e87357 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcUseBuffer)
    N:VPSS  P:2 #:00069 T:00000275a1e8e233 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcAllocBuffer)
    N:VPSS  P:2 #:00070 T:00000275a1e957db M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcFreeBuffer)
    N:VPSS  P:2 #:00071 T:00000275a1e9c7c3 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcEmptyThisBuffer)
    N:VPSS  P:2 #:00072 T:00000275a1ea3d07 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcFillThisBuffer)
    N:VPSS  P:2 #:00073 T:00000275a1eabe0f M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcTunnelRequest)
    N:VPSS  P:2 #:00074 T:00000275a1eb3e0d M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start>
    N:VPSS  P:2 #:00075 T:00000275a1ebf1af M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start>
    N:VPSS  P:2 #:00076 T:00000275a1ec6777 M:xdc.runtime.Main S:Instance Register with omxRpc Module.Cnt = 1
    N:VPSS  P:2 #:00077 T:00000275a1ecbeb3 M:xdc.runtime.Main S:L_create: OmxRpc create: Component:OMX.TI.VPSSM3.VFDC, Layer:2
    N:VPSS  P:2 #:00078 T:00000275a1ed3407 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFCC idx 0
    N:VPSS  P:2 #:00079 T:00000275a1eda04d M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.VFDC In table OMX.TI.VPSSM3.VFDC idx 1
    found handle 0x12f018 for component OMX.TI.VPSSM3.VFDC
     got display handle
    N:VPSS  P:2 #:00080 T:00000275a1ee0463 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.VFDC found idx: 1
    N:VPSS  P:2 #:00081 T:00000275a1ee7af7 M:xdc.runtime.Main S:In OMX_GetHandle, component OMX.TI.VPSSM3.VFDC, omxhandle 0x9f257f58
    N:VPSS  P:2 #:00082 T:00000275a1f4cb93 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetDefaultProperties> @line<1238>
    N:VPSS  P:2 #:00083 T:00000275a1f57bb5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> with >
    N:VPSS  P:2 #:00084 T:00000275a1f5fd37 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_ComponentInit> @line<133>
    N:VPSS  P:2 #:00085 T:00000275a1f82eb1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_InitializePorts> @line<115>
    N:VPSS  P:2 #:00086 T:00000275a206ef91 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_InitializePorts> @line<217> with error>
    N:VPSS  P:2 #:00087 T:00000275a21d1003 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_ComponentInit> @line<247> with error<0:>
    N:VPSS  P:2 #:00088 T:00000275a21e073f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00089 T:00000275a21e78f5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00090 T:00000275a21efd0b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00091 T:00000275a21f817b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00092 T:00000275a22012ef M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00093 T:00000275a2207f49 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00094 T:00000275a220fa51 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00095 T:00000275a2217bf1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00096 T:00000275a22204a5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00097 T:00000275a2226e99 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00098 T:00000275a222eab9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00099 T:00000275a2236d66 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00100 T:00000275a223f6f5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00101 T:00000275a22460e9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00102 T:00000275a22507df M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    found handle 0x135828 for component OMX.TI.VPSSM3.CTRL.DC
    N:VPSS  P:2 #:00103 T:00000275a2258aaf M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00104 T:00000275a226143b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    Buffer Size computed: 518400
    set input port params (width = 720, height = 480)
    N:VPSS  P:2 #:00105 T:00000275a2268071 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00106 T:00000275a226feff M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00107 T:00000275a227838f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00108 T:00000275a22812d5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    setting input and output memory type to default
    N:VPSS  P:2 #:00109 T:00000275a2287dbb M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00110 T:00000275a228fa41 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    enable input port
    N:VPSS  P:2 #:00111 T:00000275a2297c9b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00112 T:00000275a22a05e5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00113 T:00000275a22a6f99 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00114 T:00000275a22aebd3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00115 T:00000275a22b6e27 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00116 T:00000275a22bf539 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00117 T:00000275a22c8007 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00118 T:00000275a22cfd3b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00119 T:00000275a22d7fab M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    got eventEnable/Disable Event
    N:VPSS  P:2 #:00120 T:00000275a22e07e7 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00121 T:00000275a22e7410 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00122 T:00000275a22ef0db M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00123 T:00000275a22f75c9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00124 T:00000275a2300521 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00125 T:00000275a23070c3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00126 T:00000275a230ebfd M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00127 T:00000275a2316df3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00128 T:00000275a231f5a5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00129 T:00000275a2326064 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00130 T:00000275a232dc77 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00131 T:00000275a2335e1d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00132 T:00000275a2340505 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00133 T:00000275a2347387 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00134 T:00000275a234f2e3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00135 T:00000275a2357547 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00136 T:00000275a235fce1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00137 T:00000275a236683f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00138 T:00000275a236e9c9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00139 T:00000275a2376c73 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00140 T:00000275a237f8a3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00141 T:00000275a2386421 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00142 T:00000275a238df7b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00143 T:00000275a23960d3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00144 T:00000275a239e8e3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00145 T:00000275a23a546b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00146 T:00000275a23ad059 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00147 T:00000275a23b897f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00148 T:00000275a23c1cf5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00149 T:00000275a23c87d3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00150 T:00000275a23d07fb M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00151 T:00000275a23d8a93 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00152 T:00000275a23e1327 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00153 T:00000275a23e8305 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00154 T:00000275a23f001b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00155 T:00000275a23f82a1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00156 T:00000275a24011fb M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00157 T:00000275a2407d41 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00158 T:00000275a240f8d5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00159 T:00000275a2417c2f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00160 T:00000275a242053b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00161 T:00000275a2427027 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00162 T:00000275a242ebfb M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00163 T:00000275a24393e5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00164 T:00000275a2441ccf M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_DIO_Util> @line<546>
    N:VPSS  P:2 #:00165 T:00000275a244893d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<
    N:VPSS  P:2 #:00166 T:00000275a24508c1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_DIO_DefaultGetTotalBufferSize> @line<6>
    N:VPSS  P:2 #:00167 T:00000275a2458d1d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_DIO_Util> @line<574> with error<0:Error>
    N:VPSS  P:2 #:00168 T:00000275a2ee1239 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetCallbacks> @line<267>
    N:VPSS  P:2 #:00169 T:00000275a2ee98e7 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<0:E>
    N:VPSS  P:2 #:00170 T:00000275a2ef138b M:xdc.runtime.Main S:Result of pComponentInit: ErrorNone
    N:VPSS  P:2 #:00171 T:00000275a2ef6a65 M:xdc.runtime.Main S:Registering the component OMX.TI.VPSSM3.VFDC with TunnelMgr
    N:VPSS  P:2 #:00172 T:00000275a2efc863 M:xdc.runtime.Main S:Entered: DomxTunnelMgr_registerHandle (0x9f257f58, 0x9f704e54)
    N:VPSS  P:2 #:00173 T:00000275a2f07da7 M:xdc.runtime.Main S:Entered function:OmxRpc_rcmClientCreate (0x9f2530f8, OmxRpcRcmServer_OMX.TI.VPSSM3.)
    N:VPSS  P:2 #:00174 T:00000275a2f0fecf M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_ini>
    N:VPSS  P:2 #:00175 T:00000275a2f17233 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init>
    N:VPSS  P:2 #:00176 T:00000275a2f1e2a5 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create>
    N:VPSS  P:2 #:00177 T:00000275a2f94815 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create>
    N:VPSS  P:2 #:00178 T:00000275a2f9f2e5 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler)
    N:VPSS  P:2 #:00179 T:00000275a2fcb9ab M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone)
    N:VPSS  P:2 #:00180 T:00000275a2ff4153 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbFillBufferDone)
    N:VPSS  P:2 #:00181 T:00000275a30276dd M:xdc.runtime.Main S:Module<ti.omx> @<domxtmgr_register_skelinfo> @line<417> msg<OmxRpcRcmServer_OMX.TI.>
    N:VPSS  P:2 #:00182 T:00000275a3033483 M:xdc.runtime.Main S:OmxRpc_rcmIfGetHandle:ComponentName:OmxRpcRcmServer_OMX.TI.VPSSM3.VFDC_Ctrl_2_0.Exi.
    N:VPSS  P:2 #:00183 T:00000275ac6ffe73 M:xdc.runtime.Main S:OmxRpc_rcmIfGetHandle:ComponentName:OMX.TI.VPSSM3.CTRL.DC
    N:VPSS  P:2 #:00184 T:00000275ac70c941 M:xdc.runtime.Main S:Entered function:omxrpc_module_init_client (3)
    N:VPSS  P:2 #:00185 T:00000275ac712d95 M:xdc.runtime.Main S:LayerId: 2
    N:VPSS  P:2 #:00186 T:00000275ac71d557 M:xdc.runtime.Main S:@ omxrpc_rcm_server_create: rcmServerName OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctr4
    N:VPSS  P:2 #:00187 T:00000275ac725551 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<225> msg<Before RcmServer_Params_i>
    N:VPSS  P:2 #:00188 T:00000275ac72cbf5 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<229> msg<After RcmServer_Params_in>
    N:VPSS  P:2 #:00189 T:00000275ac733b5b M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<232> msg<Before RcmServer_create>
    N:VPSS  P:2 #:00190 T:00000275ac79a1f9 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_create> @line<240> msg<After RcmServer_create>
    N:VPSS  P:2 #:00191 T:00000275ac7a3ec1 M:xdc.runtime.Main S:@ omxrpc_rcm_server_remote_fxn_register regFxnCategory 1
    N:VPSS  P:2 #:00192 T:00000275ac7aa41b M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSetParameter)
    N:VPSS  P:2 #:00193 T:00000275ac7b4b1d M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetParameter)
    N:VPSS  P:2 #:00194 T:00000275ac7bbf3b M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSetConfig)
    N:VPSS  P:2 #:00195 T:00000275ac7c7919 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetConfig)
    N:VPSS  P:2 #:00196 T:00000275ac7ceb13 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetComponentVersion)
    N:VPSS  P:2 #:00197 T:00000275ac7d62df M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetExtensionIndex)
    N:VPSS  P:2 #:00198 T:00000275ac7dd947 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcGetState)
    N:VPSS  P:2 #:00199 T:00000275ac7e4963 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcSendCommand)
    N:VPSS  P:2 #:00200 T:00000275ac7ebc2d M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcUseBuffer)
    N:VPSS  P:2 #:00201 T:00000275ac7f399b M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcAllocBuffer)
    N:VPSS  P:2 #:00202 T:00000275ac7faf1f M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcFreeBuffer)
    N:VPSS  P:2 #:00203 T:00000275ac801fe5 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcEmptyThisBuffer)
    N:VPSS  P:2 #:00204 T:00000275ac80934d M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcFillThisBuffer)
    N:VPSS  P:2 #:00205 T:00000275ac8109b9 M:xdc.runtime.Main S:Calling RcmServer_addSymbol(OmxRpcTunnelRequest)
    N:VPSS  P:2 #:00206 T:00000275ac81857d M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<256> msg<Before RcmServer_start>
    N:VPSS  P:2 #:00207 T:00000275ac8242a9 M:xdc.runtime.Main S:Module<ti.omx> @<omxrpc_rcm_server_start> @line<258> msg<After RcmServer_start>
    N:VPSS  P:2 #:00208 T:00000275ac82b9e9 M:xdc.runtime.Main S:Instance Register with omxRpc Module.Cnt = 2
    N:VPSS  P:2 #:00209 T:00000275ac831159 M:xdc.runtime.Main S:L_create: OmxRpc create: Component:OMX.TI.VPSSM3.CTRL.DC, Layer:2
    N:VPSS  P:2 #:00210 T:00000275ac83aadb M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFCC idx 0
    N:VPSS  P:2 #:00211 T:00000275ac8418fd M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFDC idx 1
    N:VPSS  P:2 #:00212 T:00000275ac847d1b M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.DEIHDUALOUT idx 2
    N:VPSS  P:2 #:00213 T:00000275ac84e9cb M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.DEIMDUALOUT idx 3
    N:VPSS  P:2 #:00214 T:00000275ac8553d5 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.NF idx 4
    N:VPSS  P:2 #:00215 T:00000275ac85bbeb M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.VFPC.INDTXSCWB idx 5
    N:VPSS  P:2 #:00216 T:00000275ac862a33 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.CTRL.TVP idx 6
    N:VPSS  P:2 #:00217 T:00000275ac869aa9 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC In table OMX.TI.VPSSM3.CTRL.DC idx 7
    N:VPSS  P:2 #:00218 T:00000275ac8706b1 M:xdc.runtime.Main S:Component OMX.TI.VPSSM3.CTRL.DC found idx: 7
    N:VPSS  P:2 #:00219 T:00000275ac8781fb M:xdc.runtime.Main S:In OMX_GetHandle, component OMX.TI.VPSSM3.CTRL.DC, omxhandle 0x9f2807c8
    N:VPSS  P:2 #:00220 T:00000275ac88a9f7 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetDefaultProperties> @line<1238>
    N:VPSS  P:2 #:00221 T:00000275ac892717 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetDefaultProperties> @line<1280> wi>
    N:VPSS  P:2 #:00222 T:00000275ac89da73 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_ComponentInit> @line<133>
    N:VPSS  P:2 #:00223 T:00000275ac8c00d1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_InitializePorts> @line<115>
    N:VPSS  P:2 #:00224 T:00000275ac8cada9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<_OMX_BASE_InitializePorts> @line<217> with er>
    N:VPSS  P:2 #:00225 T:00000275ac921267 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_ComponentInit> @line<247> with error>
    N:VPSS  P:2 #:00226 T:00000275ac97c7ed M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SetCallbacks> @line<267>
    N:VPSS  P:2 #:00227 T:00000275ac98428d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SetCallbacks> @line<308> with error<>
    N:VPSS  P:2 #:00228 T:00000275ac98bc13 M:xdc.runtime.Main S:Result of pComponentInit: ErrorNone
    N:VPSS  P:2 #:00229 T:00000275ac990c27 M:xdc.runtime.Main S:Registering the component OMX.TI.VPSSM3.CTRL.DC with TunnelMgr
    N:VPSS  P:2 #:00230 T:00000275ac996e35 M:xdc.runtime.Main S:Entered: DomxTunnelMgr_registerHandle (0x9f2807c8, 0x9f704e54)
    N:VPSS  P:2 #:00231 T:00000275ac9a2885 M:xdc.runtime.Main S:Entered function:OmxRpc_rcmClientCreate (0x9f27bb58, OmxRpcRcmServer_OMX.TI.VPSSM3.)
    N:VPSS  P:2 #:00232 T:00000275ac9ada82 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<983> msg<Before RcmClient_Params_ini>
    N:VPSS  P:2 #:00233 T:00000275ac9b509d M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<985> msg<After RcmClient_Params_init>
    N:VPSS  P:2 #:00234 T:00000275ac9bc543 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<990> msg<Before RcmClient_create>
    N:VPSS  P:2 #:00235 T:00000275aca24bd5 M:xdc.runtime.Main S:Module<ti.omx> @<OmxRpc_rcmClientCreate> @line<992> msg<After RcmClient_create>
    N:VPSS  P:2 #:00236 T:00000275aca2f29b M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEventHandler)
    N:VPSS  P:2 #:00237 T:00000275aca5b1ff M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbEmptyBufferDone)
    N:VPSS  P:2 #:00238 T:00000275aca818b9 M:xdc.runtime.Main S:main: calling RcmClient_getSymbolIndex(OmxRpcCbFillBufferDone)
    N:VPSS  P:2 #:00239 T:00000275acaaba67 M:xdc.runtime.Main S:Module<ti.omx> @<domxtmgr_register_skelinfo> @line<417> msg<OmxRpcRcmServer_OMX.TI.>
    N:VPSS  P:2 #:00240 T:00000275acab76f7 M:xdc.runtime.Main S:OmxRpc_rcmIfGetHandle:ComponentName:OmxRpcRcmServer_OMX.TI.VPSSM3.CTRL.DC_Ctrl_2_1..
    N:VPSS  P:2 #:00241 T:00000275b6b04d17 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_GetParameter> @line<695>
    N:VPSS  P:2 #:00242 T:00000275b6b0f301 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_GetParameter> @line<858> with error<0:E>
    N:VPSS  P:2 #:00243 T:00000275b6b44ecf M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetParameter> @line<890>
    N:VPSS  P:2 #:00244 T:00000275b6b4f80b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetParameter> @line<1163> with error<0:>
    N:VPSS  P:2 #:00245 T:00000275b6bb5b93 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SetParameter> @line<890>
    N:VPSS  P:2 #:00246 T:00000275b6bbec9f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SetParameter> @line<1163> with error<0:>
    N:VPSS  P:2 #:00247 T:00000275b6beac1f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_SendCommand> @line<499>
    N:VPSS  P:2 #:00248 T:00000275b6bf74c7 M:xdc.runtime.Main S:OMX_BASE_SendCommand:OMX_CommandPortEnable, nParam1: 0
    N:VPSS  P:2 #:00249 T:00000275b6c01d2d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0:Er>
    N:VPSS  P:2 #:00250 T:00000275b6c14d6a M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434>
    N:VPSS  P:2 #:00251 T:00000275b6c1f193 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526>
    N:VPSS  P:2 #:00252 T:00000275b6c26547 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdEvent> @line<631> msg<Processing O>
    N:VPSS  P:2 #:00253 T:00000275b6c2e613 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_EnablePort> @line<777>
    N:VPSS  P:2 #:00254 T:00000275b6c35427 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_EnablePort> @line<815> with error<0:Er>
    N:VPSS  P:2 #:00255 T:00000275b6c3dd25 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CB_ReturnEventNotify> @line<100>
    N:VPSS  P:2 #:00256 T:00000275b6c48b35 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_CB_ReturnEventNotify> @line<121> msg<Notify c>
    N:VPSS  P:2 #:00257 T:00000275b6c50ea3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CB_ReturnEventNotify> @line<224> with e>
    N:VPSS  P:2 #:00258 T:00000275b6c58c4f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error>
    N:VPSS  P:2 #:00259 T:00000275b6c609c9 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<>
    N:VPSS  P:2 #:00260 T:00000275b6c69073 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdCompleteEventHandler> @line<483>
    N:VPSS  P:2 #:00261 T:00000275b6c700f1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_PROCESS_CmdCompleteEvent> @line<809>
    N:VPSS  P:2 #:00262 T:00000275b6c77821 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> @<OMX_BASE_PROCESS_CmdCompleteEvent> @line<869> msg<Proc>
    N:VPSS  P:2 #:00263 T:00000275b6c7ff9b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<_OMX_BASE_EventNotifyToClient> @line<881>
    N:VPSS  P:2 #:00264 T:00000275c0acb05f M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_SendCommand> @line<499>
    N:VPSS  P:2 #:00265 T:00000275c0ad99f5 M:xdc.runtime.Main S:OMX_BASE_SendCommand:OMX_CommandStateSet, nParam1: 2
    N:VPSS  P:2 #:00266 T:00000275c0ae4163 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Leaving<OMX_BASE_SendCommand> @line<669> with error<0>
    N:VPSS  P:2 #:00267 T:00000275c0aff527 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<_OMX_BASE_EventNotifyToClient> @line<1172> with >
    N:VPSS  P:2 #:00268 T:00000275c0b08589 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_PROCESS_CmdCompleteEvent> @line<930> wi>
    N:VPSS  P:2 #:00269 T:00000275c0b13c29 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdCompleteEventHandler> @line<496> wit>
    N:VPSS  P:2 #:00270 T:00000275c0b1c173 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Entering<OMX_BASE_CmdEventHandler> @line<434>
    N:VPSS  P:2 #:00271 T:00000275c0b240c1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.VFDC> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<>
    N:VPSS  P:2 #:00272 T:00000275c0b2eef5 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_CmdEventHandler> @line<434>
    N:VPSS  P:2 #:00273 T:00000275c0b38bd3 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<OMX_BASE_PROCESS_CmdEvent> @line<526>
    N:VPSS  P:2 #:00274 T:00000275c0b4063b M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> @<OMX_BASE_PROCESS_CmdEvent> @line<538> msg<Processin>
    N:VPSS  P:2 #:00275 T:00000275c0b486a1 M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> Entering<_OMX_BASE_HandleStateTransition> @line<316>
    N:VPSS  P:2 #:00276 T:00000275c0b4f61d M:xdc.runtime.Main S:Module<OMX.TI.VPSSM3.CTRL.DC> @<_OMX_BASE_HandleStateTransition> @line<339> msg<Loa>
    N:VPSS  P:2 #:00277 T:00000275c0b8e349 M:xdc.runtime.Main S:FATAL ERROR: ErrorCode:0x1. Unhandled Exception:
    N:VPSS  P:2 #:00278 T:00000275c0b94ca3 M:xdc.runtime.Main S:Exception occurred in ThreadType_Task
    N:VPSS  P:2 #:00279 T:00000275c0b99e5b M:xdc.runtime.Main S:handle: 0x9f283af8.
    N:VPSS  P:2 #:00280 T:00000275c0b9e9b3 M:xdc.runtime.Main S:stack base: 0x9f2812f0.
    N:VPSS  P:2 #:00281 T:00000275c0ba38cd M:xdc.runtime.Main S:stack size: 0x2800.
    N:VPSS  P:2 #:00282 T:00000275c0ba834f M:xdc.runtime.Main S:R0 = 0xd1042800  R8  = 0x9f5f20f8
    N:VPSS  P:2 #:00283 T:00000275c0badbe9 M:xdc.runtime.Main S:R1 = 0x0000000c  R9  = 0x9f22d8d4
    N:VPSS  P:2 #:00284 T:00000275c0bb3187 M:xdc.runtime.Main S:R2 = 0x00000001  R10 = 0x80001001
    N:VPSS  P:2 #:00285 T:00000275c0bb8a93 M:xdc.runtime.Main S:R3 = 0x9f235894  R11 = 0x9f5f2250
    N:VPSS  P:2 #:00286 T:00000275c0bbe06d M:xdc.runtime.Main S:R4 = 0x00000000  R12 = 0x00000018
    N:VPSS  P:2 #:00287 T:00000275c0bc35bd M:xdc.runtime.Main S:R5 = 0x00000000  SP(R13) = 0x9f283880
    N:VPSS  P:2 #:00288 T:00000275c0bc8b6b M:xdc.runtime.Main S:R6 = 0x00000000  LR(R14) = 0x9f65395d
    N:VPSS  P:2 #:00289 T:00000275c0bce3c3 M:xdc.runtime.Main S:R7 = 0x9f22d8d8  PC(R15) = 0x9f66959a
    N:VPSS  P:2 #:00290 T:00000275c0bd3b9f M:xdc.runtime.Main S:PSR = 0x01000000
    N:VPSS  P:2 #:00291 T:00000275c0bd868b M:xdc.runtime.Main S:ICSR = 0x0440f803
    N:VPSS  P:2 #:00292 T:00000275c0bdd17b M:xdc.runtime.Main S:MMFSR = 0x00
    N:VPSS  P:2 #:00293 T:00000275c0be1799 M:xdc.runtime.Main S:BFSR = 0x82
    N:VPSS  P:2 #:00294 T:00000275c0be5d2b M:xdc.runtime.Main S:UFSR = 0x0000
    N:VPSS  P:2 #:00295 T:00000275c0bea5dd M:xdc.runtime.Main S:HFSR = 0x40000000
    N:VPSS  P:2 #:00296 T:00000275c0beee65 M:xdc.runtime.Main S:DFSR = 0x00000000
    N:VPSS  P:2 #:00297 T:00000275c0bf3915 M:xdc.runtime.Main S:MMAR = 0xd1042800
    N:VPSS  P:2 #:00298 T:00000275c0bf8365 M:xdc.runtime.Main S:BFAR = 0xd1042800
    N:VPSS  P:2 #:00299 T:00000275c0bfce97 M:xdc.runtime.Main S:AFSR = 0x00000000
    N:VPSS  P:2 #:00300 T:00000275c0c0156b M:xdc.runtime.Main S:FATAL ERROR: ErrorCode:0x1. Terminating Execution...

    Regards,

    Geetha

  • Hello,

    Check these thread:
    e2e.ti.com/.../845454
    e2e.ti.com/.../208103
    e2e.ti.com/.../206397

    The composite output should work in 5.05.02.

    BR
    Margarita
  • Hi Margaita,


    Already we have tried options mentioned in the above links


    FYI: The commands used to enable SD output

    echo 0 > /sys/devices/platform/vpss/display2/enabled
    echo svideo > /sys/devices/platform/vpss/display2/output
    echo 1 > /sys/devices/platform/vpss/display2/enabled
    echo 0 > /sys/devices/platform/vpss/graphics0/enabled
    echo 1:sd > /sys/devices/platform/vpss/graphics0/nodes
    echo 1 > /sys/devices/platform/vpss/graphics0/enabled

    Still the display application hangs.


    Please help us in resolving the issue.

    Regards,

    Geetha Rajammal.M