This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM572x interface to ADV7343

Hi All

We are going to use ADV7343 for encoding 24-bit RGB out from LCD3 port to PAL. This encoder accepts RGB as input. But if we are giving input as progressive, it recommends 720x288@50Hz.

AM5728------>LCD3 Out(24 lines)----->ADV7343---->PAL

How can i configure this output resolution in device tree?

I have already written the driver for this by taking the help from panel-dpi driver  and configured the same in device tree. Only resolution settings are left.

Regards

Amrit