I have a AM5728 Customize board, and I want to boot from QSPI flash In Raw(UDA) mode.
I have configured the sysboot pin according to the following picture
What configuration I should do for SPL ? because I have seen the MLO.byteswap in AM335x platform. and
not seen the image for AM57xx. The MLO image can be used for QSPI boot ?
If it's OK, How can I setting Configuration header for QSPI in SPL source code ?
Thank you very much !
Best Regards
Qing