This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The sample of SPI on C6748 LCDk.

I'm sorry my English is not good .My company bought a board of C6748 LCDK,  and I use is that you provide the sample code.The address is:C:\ti\C6748_StarterWare_1_20_04_01\examples\lcdkC6748\spi .I have the code will burn to we in the design of the circuit board.Our board is modeled after you give the schematic diagram of design.After burning,SPI_SIMO on the oscilloscope have no reaction, because of your C6748 LCDK board SPI1 connection to J16. I don't have that kind of adapter plate.I will change SPI0 SOC_SPI_1_REGS and some other parameters, burn to LCDK development board, the result is the same, I  have already connect 0 ohms resistors for R214,R215,R216 and remove R184,R179,and R178....What reason is this excuse me?