Other Parts Discussed in Thread: AM3351
In our custom board based on am3351, we have connected a Switch to GPIO1_29. The switch circuit is shown as below
In dts, I configured the GPIO1_29 as follow
media_keys_s0: media_keys_s0 {
pinctrl-single,pins = <
0x7c ( PIN_INPUT_PULLUP | MUX_MODE7 ) /* gpmc_csn0.gpio1[29] */
};
gpio_keys: volume_keys@0 {
compatible = "gpio-keys";
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&media_keys_s0>;
switch@1 {
label = "playlist";
linux,code = <163>;
gpios = <&gpio1 29 GPIO_ACTIVE_LOW>;
gpio-key,wakeup;
};
};
After device boot, I tried to capture the input event of the switch. But it is not sending any event to userspace. During switch press, I directly read the GPIO input data register(devmem2 0x4804C138), it always show high for GPIO1_29 pin, except one or two times it goes to zero. Then I manually exported the GPIO1_29 using sys/class/gpio (only mux configuration added into dts). Now I was able to toggle the GPIO1_29 pin by configuring the direction as output. But when I set the direction as input, the value always shows high during switch press, except one or two times it goes to zero.