Other Parts Discussed in Thread: OMAPL138
OMAP-L138-EP
CCS 6.x
Starterware 1.10.04.01
All:
There is a new spin of a board coming my way that uses several pins normally associated with EMIFA.
On this board, EMIFA is connected to NAND Flash (similar to that used on LCDK board). I use Starterware NAND flash testing as part of board testing, and I want to confirm that the NANDPinMuxSetup( ) only uses EMA_A[1] and EMA_A[2] in conjunction with NAND interface, essentially allowing use of all of the other EMA_A pins as GPIO. (It looks like the LCDK itself only uses a subset of the available EMA_A bus and brings several (unused) pins to a header.