This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

support for 3-wire ?

Guru 20755 points

Hello,

We use 3-wire rtc, but it does not work.

I am not sure that 3-wire is supported with chip (omap2_spi).

Is it supported ?

Regards,

Ran

  • Ran,

    3-wire seems to be controlled from the below DM814x McSPI register bits:

    MCSPI_CH(i)CONF

    [18] IS - Input select
    0x0: Data line 0 (SPI_D[0]) selected for reception.
    0x1: Data line 1 (SPI_D[1]) selected for reception.

    [17] DPE1 - Transmission enable for data line 1
    0x0: Data line 1 (SPI_D[1]) selected for transmission
    0x1: No transmission on data line 1 (SPI_D[1])

    [16] DPE0 - Transmission enable for data line 0
    0x0: Data line 0 (SPI_D[0]) selected for transmission
    0x1: No transmission on data line 0 (SPI_D[0])

    [13:12] TRM - Transmit/receive modes
    0x0: Transmit and receive mode
    0x1: Receive-only mode
    0x2: Transmit-only mode

    You will need to adjust the McSPI driver (drivers/spi/omap2_mcspi.c) according to your specific use case.

    #define OMAP2_MCSPI_CHCONF_TRM_RX_ONLY BIT(12)
    #define OMAP2_MCSPI_CHCONF_TRM_TX_ONLY BIT(13)
    #define OMAP2_MCSPI_CHCONF_TRM_MASK (0x03 << 12)

    #define OMAP2_MCSPI_CHCONF_DPE0 BIT(16)
    #define OMAP2_MCSPI_CHCONF_DPE1 BIT(17)
    #define OMAP2_MCSPI_CHCONF_IS BIT(18)

    Adjust functions omap2_mcspi_setup_transfer().

    Note also that this driver is updated in more recent kernels (3.x, 4.x), it is now named spi-omap2-mcspi.c and is updated like:

    /* standard 4-wire master mode: SCK, MOSI/out, MISO/in, nCS
    * REVISIT: this controller could support SPI_3WIRE mode.
    */
    if (mcspi->pin_dir == MCSPI_PINDIR_D0_IN_D1_OUT) {
    l &= ~OMAP2_MCSPI_CHCONF_IS;
    l &= ~OMAP2_MCSPI_CHCONF_DPE1;
    l |= OMAP2_MCSPI_CHCONF_DPE0;
    } else {
    l |= OMAP2_MCSPI_CHCONF_IS;
    l |= OMAP2_MCSPI_CHCONF_DPE1;
    l &= ~OMAP2_MCSPI_CHCONF_DPE0;
    }

    Regards,
    Pavel
  • Hi Pavel,

    Thank you for the pointers.
    I understand from this that the updated version does not support 3-wire...


    Thanks,
    Ran