Hi there, I am using the NSP 1_10_03_15 and NDK 2_25_0_09 and I am trying to understand how to write applications based on the socket programming. While reading the user/design guide and reference guide... I realised the the recommended way to program is using BSD compatible API. Now I am trying to convert the helloWorld example so that it used BSD compatible API and I am following the Section 3.3 in the reference guide by not sure if there is an example already out there? Is there any example design which uses BSD compatible API for socket programming?
Regards,
Mitesh