This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Undefined symbols linking failure for DSPLink samples build

Other Parts Discussed in Thread: OMAP3530

Hi,

This is the overall procedure I followed to this point

  1. From $OEHOME/build executed bitbake ti-codec-engine. Installed correctly
  2. Followed instructions at http://code.google.com/p/opencv-dsp-acceleration/wiki/GettingStarted1 detailed below
  3. Installed following tools in a local dir called Work :
    bios : 5_33_04        codec_engine : 2_24_01      dsplink : 1_61_03       ti_cgt_c6000 : 6.1.9           xdctools : 3_15_01_59
  4. DSPLink config executed as:  perl dsplinkcfg.pl --platform=OMAP3530 --nodsp=1  --dspcfg_0=OMAP3530SHMEM     --dspos_0=DSPBIOS5XX --gppos=OMAPLSP --comps=ponslrmc --DspTskMode=1
  5. Make files edited to map directory paths to current settings
  6. Able to make files in following directories : $DSPLINK/gpp/src/api/  $DSPLINK/gpp/src   $DSPLINK/gpp/src/samples  $DSPLINK/dsp/src/
  7. make -s command from $DSPLINK/dsp/src/samples which is supposed to build the .outs for sample apps fails due to Undefined symbols. A few of the errors is shown below

             CLK_A_TABBEG   /home/jars/Work/dsplink/dsplink_1_61_03/dsplink/dsp/BUILD/OMAP3530_0/LOOP/OBJ/DEBUG/loopcfg.obj                

              _KNL_curtask        /home/jars/Work/dsplink/dsplink_1_61_03/dsplink/dsp/BUILD/OMAP3530_0/EXPORT/DEBUG/dsplinkmpcs.lib<mpcs.obj>  

             _DDR2                    /home/jars/Work/dsplink/dsplink_1_61_03/dsplink/dsp/BUILD/OMAP3530_0/LOOP/OBJ/DEBUG/swiLoop.obj

             _GBL_freq              /home/jars/Work/dsplink/dsplink_1_61_03/dsplink/dsp/BUILD/OMAP3530_0/EXPORT/DEBUG/dsplink.lib<dsplink.obj>

 

I've seen Kev and Richard face the same problems with OMAPL137 but their fixes were for Windows

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/29344/102054.aspx#102054
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/33866/117818.aspx#117818

I'm not sure as to how I can edit the files that are linking these symbols, perhaps some headers are missing? Any pointers? I've double checked my paths and they all seem correctly set.

Thanks

Mel