Other Parts Discussed in Thread: OMAP-L138, OMAPL138
I failed to load my test code to my TI LCDKOMAPL138 board. see error message below. But I have not problem to load code to my Logic PD - Zoom™ OMAP-L138 eXperimenter Kit. both boards use OMAP-L138 DSP.
using the same GEL file. does this indicate a hardware issue?
C674X_0: Output: Target Connected.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: Memory Map Cleared.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: Memory Map Setup Complete.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: PSC Enable Complete.
C674X_0: Output: ---------------------------------------------
C674X_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz
C674X_0: Output: DDR initialization is in progress....
C674X_0: Trouble Writing Memory Block at 0x1e1a110 on Page 0 of Length 0x4: (Error -1137 @ 0x1E1A110) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.1.507.0)
C674X_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01E1A110 at *((unsigned int *) (0x01E1A000+0x110))=PLLM [C6748_LCDK.gel:43] at device_PLL1(24, 1, 0, 1, 2) [C6748_LCDK.gel:406] at Set_DDRPLL_150MHz() [C6748_LCDK.gel:424] at Set_DDR2_150MHz() [C6748_LCDK.gel:459] at Core_300MHz_mDDR_150MHz() [C6748_LCDK.gel:245] at OnTargetConnect() .
Thanks in advance!
Ron