Hello,
We are considering implementing the following architecture on a AM5728:
- 2 EtherCat Slaves interfaces on PRU2, driven by the first M4
 - 1 EtherCat Master interface on PRU1 (PRU1 would actually be a standard Ethernet), driven by the second M4
 - 1 Gigabit Ethernet interface on GMAC accessed by Cortex A15
 
Because GMAC and PRU1 pins are multiplexed, do you see any concern with the following routing used concurrently:
- PRU2ETH0 for Slave EtherCat
 - PRU2ETH1 for Slave EtherCat
 - PRU1ETH1 for Master EtherCat
 - RGMII0 for Gigabit interface
 
We would test this configuration using AM5728 Industrial EVM.
Thank you for your feedback.
AM5728_User