Simple question I hope. I am using ccsv5 and recent BIOS and PDK downloads, etc..
I noticed that there are quite a few 'example' directories that will not work with the 'import a CCS project' mechanism.
One example is /ti/pdk_C6678_1_1_2_6/packages/ti/drv/srio/example/SRIOMulticoreLoopback
It contains source files, a linker file and
SRIO_MulticoreLoopbackexampleProject.txt
which is a list of the files in the directory and some hints for the compiler command line.
How do I import this into CCSv5 - there is no .cdt, .project, .cproject, etc file for the ccsv5 browser to key on.
Are these examples from older tools usage or am I missing the proper methodology ?
Thanks