This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ERROR while installing CC studio for 6713

Whie Installation of CC studio for 6713 Iam getting the error as "Error:1406; Could not write value to key Software/classes\CDB.  Verify that you have sufficient access to key...or contact your support personnel" I tried to install in administrator...But Iam getting the error again after re installing also

  • What version of CCS are you trying to install and what is your host configuration? From the error indicated, it appears to be a windows machine ..but make sure you read the compatability information provided in the Release notes of CCS before installing on the machine.
  • Hi Parag,

    Are you trying to install the licensed version of CCS?

    1. Specify your CCS version, the operating system of your host PC etc.

    2. Please visit this wiki in which the system requirement is given against each version of CCS.

    For example, if the CCS version is 6, the below is the system requirement.

    Hardware Requirements

    Minimum Recommended
    Memory 4GB 6GB
    Disk space 400MB* 2GB
    Processor 1.0GHz x86 compatible processor Dual core x86 compatible processor
    • Disk space listed depends on features selected during installation. 400MB is for a bare minimal installation. Does not include temporary space required by the installer.
    • Note that the most important requirement is memory. At least 2GB of memory or more memory is highly recommended.

    Operating System Requirements

    • Windows: XP SP3, Windows 7 (SP1 or later) and Windows 8.x is supported by all CCSv6 versions. Windows 10 is supported by CCS versions 6.1.3 and greater
    • Linux: details on the Linux distributions supported is available here
    • Mac: MacOS is supported by CCS versions 6.1.3 and greater