This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138/AM1808 SDK

Other Parts Discussed in Thread: OMAP-L138, OMAPL138, DA8XX

I'm starting the software effort for a custom board based (to some extent) on the Logic PD L138 SOM / Baseboard.  I downloaded DaVinci-PSP-SDK-03.20.00.12.tgz and extracted the files to rebuild U-Boot as instructed here:

http://processors.wiki.ti.com/index.php/GSG:_Building_Software_Components_for_OMAP-L1#Rebuilding_U-Boot

I noticed that tar files within the DaVinci-PSP-SDK-03.20.00.12.tgz do not get extracted.  This may be by design, but is confusing.  I extracted u-boot-03.20.00.12.tar.gz and was able to rebuild the bootloader.

Questions:

1.  Is DaVinci-PSP-SDK-03.20.00.12.tgz the place to start for the SDK?

2.  http://processors.wiki.ti.com/index.php/GSG:_Building_Software_Components_for_OMAP-L1#Rebuilding_U-Boot says that patches have already been applied, but the /src/u-boot directory contains u-boot-patches-03.20.00.12.tar.gz.  Should I ignore it or extract it?  There's also a Unified-patch-03.20.00.12.gz.