Other Parts Discussed in Thread: AM3517, TSC2004, TVP5146
Hello,
I created a jffs image from my nfs directory with the command:
mkfs.jffs2 -lqnp -e 128 -r $HOME/nfs -o jffs
Later i've written that jffs and the uImage(this works ok with nfs) on flash:
Everything is ok till here. But the boot process stucks at some point after "run nandboot" command. The content of the command is:
nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr} and
nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2 omapfb.vram=0:1M
The console output is:
Booting from nand ...
NAND read: device 0 offset 0x280000, size 0x400000
4194304 bytes read: OK
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-2.6.32
Image Type: ARM Linux Kernel Image (uncompre
ssed)
Data Size: 2310640 Bytes = 2.2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux................................................................................................................................................. done, booting the kernel.
Linux version 2.6.32 (root@linux-yigit) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #6 Mon May 31 14:56:02 EEST 2010
CPU: ARMv7 Processor [411fc087] revision 7 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3517/AM3517 EVM
Memory policy: ECC disabled, Data cache writeback
AM3517 ES1.0 (l2cache iva sgx neon isp )
SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000
Reserving 4194304 bytes SDRAM for VRAM
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
Kernel command line: console=ttyS2,115200n8 root=/dev/mtdblock4 rw rootfstype=jffs2 omapfb.vram=0:1M
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 256MB = 256MB total
Memory: 250880KB available (4016K code, 377K data, 164K init, 0K highmem)
Hierarchical RCU implementation.
NR_IRQS:368
Clocking rate (Crystal/Core/MPU): 26.0/332/500 MHz
GPMC revision 5.0
IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
Total of 96 interrupts on 1 active controller
OMAP GPIO hardware version 2.5
OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
regulator: core version 0.5
NET: Registered protocol family 16
mux: Could not set signal i2c2_scl
mux: Could not set signal i2c2_sda
mux: Could not set signal i2c3_scl
mux: Could not set signal i2c3_sda
Display initialized successfully
OMAP DMA hardware revision 4.0
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c_omap i2c_omap.1: bus 1 rev3.12 at 400 kHz
regulator: VDCDC1: 1200 mV normal
regulator: VDCDC2: 3300 mV normal
regulator: VDCDC3: 1800 mV normal
regulator: LDO1: 1800 mV normal
regulator: LDO2: 3300 mV normal
i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
input: Unspecified device as /class/input/input0
Switching to clocksource 32k_counter
musb_hdrc: version 6.0, cppi4.1-dma, otg (peripheral+host), debug=0
AM3517 OTG revision 4ea41001, PHY f0036a2, control 00
musb_hdrc: USB OTG mode controller at d0810000 using DMA, IRQ 71
NET: Registered protocol family 2
IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
AM3517 Linux PSP version 03.00.00.05 (AM3517EVM)
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
msgmni has been set to 490
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
OMAP DSS rev 2.0
OMAP DISPC rev 3.0
OMAP VENC rev 2
OMAP DSI rev 1.0
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
serial8250.1: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
serial8250.2: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
console [ttyS2] enabled
brd: module loaded
loop: module loaded
omap2-nand driver initializing
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
Creating 5 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000080000 : "xloader-nand"
0x000000080000-0x000000240000 : "uboot-nand"
0x000000240000-0x000000280000 : "params-nand"
0x000000280000-0x000000780000 : "linux-nand"
0x000000780000-0x000020000000 : "jffs2-nand"
vcan: Virtual CAN interface driver
CAN device driver interface
TI High End CAN Controller Driver 0.7
ti_hecc ti_hecc.1: device registered (reg_base=d0878000, irq=24)
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver dm9601
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: OMAP-EHCI Host Controller
usb usb1: Manufacturer: Linux 2.6.32 ehci_hcd
usb usb1: SerialNumber: ehci-omap.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 3 ports detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbtest
g_ether gadget: using random self ethernet address
g_ether gadget: using random host ethernet address
usb0: MAC 9e:a4:b8:40:32:16
usb0: HOST MAC 72:eb:30:8d:be:df
g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
g_ether gadget: g_ether ready
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 2.6.32 musb-hcd
usb usb2: SerialNumber: musb_hdrc
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
input: TSC2004 Touchscreen as /class/input/input1
rtc-s35390a 1-0030: rtc core: registered rtc-s35390a as rtc0
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
vpfe_init
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
tvp514x 3-005c: tvp514x 3-005c decoder driver registered !!
vpfe-capture vpfe-capture: v4l2 sub device tvp5146 registered
vpfe_register_ccdc_device: DM6446 CCDC
DM6446 CCDC is registered with vpfe.
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Advanced Linux Sound Architecture Driver Version 1.0.21.
usbcore: registered new interface driver snd-usb-audio
No device for DAI tlv320aic23
No device for DAI omap-mcbsp-dai-0
No device for DAI omap-mcbsp-dai-1
No device for DAI omap-mcbsp-dai-2
No device for DAI omap-mcbsp-dai-3
No device for DAI omap-mcbsp-dai-4
OMAP3517 / AM3517 EVM SoC init
AIC23 Audio Codec 0.1
asoc: tlv320aic23 <-> omap-mcbsp-dai-0 mapping ok
ALSA device list:
#0: am3517evm (tlv320aic23)
TCP cubic registered
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Power Management for TI OMAP3.
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
regulator_init_complete: incomplete constraints, leaving LDO2 on
regulator_init_complete: incomplete constraints, leaving LDO1 on
davinci_emac_probe: using random MAC addr: 92:fd:fb:58:58:cc
emac-mii: probed
rtc-s35390a 1-0030: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
omap_vout omap_vout: Buffer Size = 3686400
omap_vout omap_vout: : registered and initialized video device 1
omap_vout omap_vout: Buffer Size = 3686400
omap_vout omap_vout: : registered and initialized video device 2
Empty flash at 0x167938e0 ends at 0x16794000
JFFS2 error: (1) jffs2_build_inode_pass1: child dir "lib" (ino #1258) of dir ino #1255 appears to be a hard link
JFFS2 error: (1) jffs2_build_inode_pass1: child dir "plugins" (ino #1259) of dir ino #1255 appears to be a hard link
VFS: Mounted root (jffs2 filesystem) on device 31:4.
Freeing init memory: 164K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
/etc/rcS.d/S03udev: line 36: awk: Permission denied
/etc/rcS.d/S03udev: line 50: cmp: Permission denied
Populating dev cachetar: dev/log: socket ignored
/etc/rcS.d/S10checkroot: line 192: awk: Permission denied
Remounting root file system...
/etc/rcS.d/S30ramdisk: line 13: cut: Permission denied
/etc/rcS.d/S30ramdisk: line 13: cut: Permission denied
0: mount: mounting rootfs on / failed: No such file or directory
0: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
0: mount: mounting tmpfs on /dev/shm failed: No such file or directory
/etc/init.d/rc: /etc/rcS.d/S35mountall.sh: line 58: awk: Permission denied
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
chown: unknown user/group root:root
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:00, id=7c0f1)
udhcpc (v1.13.2) started
udhcpc: exec /usr/share/udhcpc/default.script: Not a directory
Sending discover...
PHY: ffffffff:00 - Link is Up - 100/Full
Sending discover...
Sending discover...
udhcpc: exec /usr/share/udhcpc/default.script: Not a directory
No lease, failing
done.
/sbin/ldconfig: /usr/lib/libQtCore.so.4 is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: /usr/lib/libGLESv2.so.1.1.14.2616 is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: File /usr/lib/libGLESv2.so is empty, not checked.
/sbin/ldconfig: File /usr/lib/libOpenVGU.so is empty, not checked.
/sbin/ldconfig: /usr/lib/libOpenVG.so.1.1.14.2616 is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: /usr/lib/libIMGegl.so.1.1.14.2616 is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: /usr/lib/libIMGegl.so is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: File /usr/lib/libOpenVG.so is empty, not checked.
/sbin/ldconfig: File /usr/lib/libasound.so.2 is empty, not checked.
/sbin/ldconfig: /usr/lib/libGLES_CM.so.1.1.14.2616 is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: /usr/lib/libGLES_CM.so is not an ELF file - it has the wrong magic bytes at the start.
/sbin/ldconfig: File /usr/lib/libPVRScopeServices.so is empty, not checked.
/sbin/ldconfig: file /usr/lib/libasound.so.2.0.0 is truncated
/sbin/ldconfig: /usr/lib/libPVRScopeServices.so is not a symbolic link
/sbin/ldconfig: /usr/lib/libOpenVGU.so is not a symbolic link
/etc/init.d/rc: /etc/rcS.d/S55bootmisc.sh: line 79: awk: Permission denied
expr: syntax error
sh: 1: unknown operand
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd/usr/sbin/thttpd: unknown user - 'nobody'
.
INIT: no more processes left in this runlevel
JFFS2 notice: (1262) check_node_data: wrong data CRC in data node at 0x167935b0: read 0x45760327, calculated 0x14d6f7aa.
At this point boot process stucks. I am using AM35x-OMAP35x-PSP-SDK-03.00.00.05 and U-Boot 2009.08-dirty (Jan 05 2010 - 10:21:46). This filesytem and kernel image works correctly with nfs. What may be the problem?
Thanks in advance..
Yigit