This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2L06 clock questions

Other Parts Discussed in Thread: 66AK2L06

I need some help understanding the clock input requirements for the 66AK2L06 DSP as stated in the "Hardware Design Guide for Keystone II Devices" (SPRAVB0):

 

1) PCIECLK: In Table 6, the valid clock frequency is stated as 100MHz, but Table 20 states the three valid clocks as 156.25MHz, 250MHz & 312.5MHz. Which table is correct?

 

2) SGMIICLK: In Table 6, the valid clock frequency is stated as 125MHz, but Table 15 states the three valid clocks as 156.25MHz, 250MHz & 312.5MHz. Which table is correct?

 

3) Is CORECLK in table 4 the same as SYSCLK in table 6?

 

4) SYSCLK: Table 6 states valid input frequencies of 122.88MHz, 153.60MHz and 307.20MHz, but I believe these only apply if the AIF (antenna interface) is used. We're not using AIF, so SYSCLK can be anything between 40MHz & 312.5MHz per table 4, is that correct?