The bootloader display driver and splash image is loading just fine, but right before the OS loads, the display is being cleared. The result is that the splash screen is shown during boot but there is about a two second window where the screen is blank. It looks sloppy. I'd like to change the display driver, but I'm not sure where this is happening.
In the windows CE forums, they are saying that the display driver should be modified, any ideas on what clears the framebuffer in the display driver during the transition from the bootloader to the OS?