Hello,
i have the sitara processor ti4376. we want to use both ethernet-ports of the processor. But on one port we can just receive messages but not send. To send messages, the internal MAC of the processor needs to know, on which port the message should be send out. therefor there is a TX-Buffer Descriptor (data-sheet "spruhl7d" chapter 15.3.2.4.1.1) where i can enter in the 16 & 17 Bit of the Descriptor, on which port the message should be sent. So why do i need to specify a VLAN-ID (in the ALE-Registers) for the internal switch in the MAC of the Processor, when i can set up the correct port in the cpdma TX interface?
Thanks a lot!
best regards
Reiner