Other Parts Discussed in Thread: OMAPL138
Hello
Am using omapl138 evm board i have an error whilw booting through the sd card in the tera term am geting these can anybody help to boot through the sd card.
pArgs->flags............. 0x9
pArgs->devLoc.IfcType.... 0
pArgs->devLoc.LogicalLoc. 0x1E23000
pArgs->devLoc.PhysicalLoc 0x0
pArgs->devLoc.Pin........ 0
pArgs->ip4address........ 1
pDevice->Name............ s
pDevice->ifcType......... 0
pDevice->id.............. 0x1E23000
pDevice->resource........ 0
pDevice->type............ 2
pDevice->pDriver......... 0x80C39000
MAC addr is 0:8:ee:3:b0:11.
OMAPEmacInit: f_pEmacRxDesc = 0xb0620000
OMAPEmacInit: f_pEmacTxDesc = 0xb0621000
OMAPEmacInit: waiting for active phy...
OMAPEmacInit: f_pMdioRegs->m_Alive = 0x1
KITL: *** Device Name OMAPL138-45073 ***
KITL: using sysintr 0x11
VBridge:: built on [Jun 4 2010] time [16:24:03]
VBridgeInit()...TX = [16384] bytes -- Rx = [16384] bytes
Tx buffer [0xA0C6FCA0] to [0xA0C73CA0].
Rx buffer [0xA0C73CC0] to [0xA0C77CC0].
VBridge:: NK add MAC: [0-8-EE-3-B0-11]
Connecting to Desktop
Connecting to Desktop .. resending
Connecting to Desktop .. resending
Regards
Vinoth,