This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM572x USB 3.0 direct to connector

Other Parts Discussed in Thread: AM5728

Hi all

We're going to use AM5728's USB port 1 in 3.0 SuperSpeed mode to host a high resolution camera. Since that camera is the only endpoint, I don't really need a hub. So can the AM5728 be tied directly to the USB connector?  Any risks to doing so (yes, there will be TVS diodes)?

Thanks!

MADman