This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DA810] undershoot voltage level for input signal

Hi

My customer has a question about the allowed undershoot voltage level for incoming signal on DA810. In the datasheet, there is a spec for output signal (Transient Overshoot/Undershoot) and that is 20% DVDD during 20% signal frequency, but no spec for input. I found the same question here, but it is for OMAPL-138.

Can I understand the same is applicable to DA810 except for 1.8V related descriptions ? DA810 is no support for dual voltage and it only support 3.3V IO voltage. 

Best Regards,
Naoki