Other Parts Discussed in Thread: TDA2, TDA2E
Hi,
We have project on having 3 or 4 HD Ethernet connection camera for Automotive and need to be display on LCD screen.
Format output from HD Camera will be MJPEG or H.264 in AVB packet ot RTP packet.
Frame size are 1080 x 720 with 30fps (can be adjust base on requirement.
All the camera will input to a 4 port switch and having 1 output RGMII to CPU and display on the screen.
The project are similar to Arround View Monitor, however on the LCD will have 3 section to display individual camera picture.
The main task of the processor will be received the packet -> reconstruct the packet become a valid frame -> decode the frame -> rescale to LCD section size -> convert to RGB and display on LCD.
1) Did TDA2 or TDA2e are capable on handling the processing of the MJPEG and H.264 for 4 camera with no frame drop problem?
2) Any parts that can be recommend to me?
3) For TDA2 or TDA2e, what will be the OS using?
4) What is the bundle of the whole Evaluation Kit + Software part number sot that I can get quote from Avnet Supplier?
5) Any tranining material that I can refer to for the TDA2 or TDA2e, so that I can get more understand of the product.
Thanks
KJ Lee