Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Dear all :
I debug the program on XOMAP chips ( my own boards, not the EVM ), and I re-designed the PCB for the second version, the L138 new chips I got is OMAP. when I debug the new boards, the problem came. it is: when I setup the PLL0 to 300MHz ( DSP side), the ARM report error , pls see the follow:
Warning: 0x60000060/-1029 @ marker 11103 Error during: Execution, Initialization, The ICECrusher register scan returned invalid data
the error comes everytime when I excute :
// lock pll regs.
SETBIT(SYSCONFIG->CFGCHIP[0], PLL0_MASTER_LOCK);
in PLL0 setup program.
the XOMAP chip is : XOMAPL138ZWT $7-95A6PGW G1
the OMAP chip is: OMAPL13AZWT $7-9CA9Q9WFR G1
Now , the OMAPL138 in my new board can only run upto about 150MHz.