Other Parts Discussed in Thread: TPS65910
Hi all,
I have a custom board with am335x on it.
I'm running linux 3.12.10-ti2013.12.01 from SDK 07.00.00.00.
Standby mode fails:
echo standby > /sys/power/state
-sh: echo: write error: No such device
The reason seems to be an i2c-problem.
During boot this msg appears:
[ 1.891638] Error fetching I2C sleep/wake sequence
In my bootlog also this warning appears:
[ 1.717946] ------------[ cut here ]------------ [ 1.722857] WARNING: CPU: 0 PID: 1 at arch/arm/mach-omap2/omap_device.c:888 omap_device_get_by_hwmod_name+0x94/0xb4() [ 1.734002] omap_device_get_by_hwmod_name: no omap_device for i2c1 [ 1.740490] Modules linked in: [ 1.743705] CPU: 0 PID: 1 Comm: swapper Not tainted 3.12.10-ti2013.12.01 #5 [ 1.751020] Backtrace: [ 1.753598] [<c0017880>] (dump_backtrace+0x0/0x10c) from [<c0017a1c>] (show_stack+0x18/0x1c) [ 1.762456] r6:c002f564 r5:00000009 r4:ed083e28 r3:00000000 [ 1.768421] [<c0017a04>] (show_stack+0x0/0x1c) from [<c05d0a08>] (dump_stack+0x20/0x28) [ 1.776840] [<c05d09e8>] (dump_stack+0x0/0x28) from [<c0046d08>] (warn_slowpath_common+0x70/0x90) [ 1.786164] [<c0046c98>] (warn_slowpath_common+0x0/0x90) from [<c0046dcc>] (warn_slowpath_fmt+0x38/0x40) [ 1.796134] r8:c07db3fc r7:c07d8410 r6:c11c2744 r5:c097f508 r4:c0717d64 [ 1.803198] [<c0046d94>] (warn_slowpath_fmt+0x0/0x40) from [<c002f564>] (omap_device_get_by_hwmod_name+0x94/0xb4) [ 1.813972] r3:c05dbe84 r2:c071434c [ 1.817748] [<c002f4d0>] (omap_device_get_by_hwmod_name+0x0/0xb4) from [<c07e8280>] (am33xx_pm_init+0x204/0x45c) [ 1.828432] r4:00000000 [ 1.831105] [<c07e807c>] (am33xx_pm_init+0x0/0x45c) from [<c07e0c00>] (am33xx_init_late+0x18/0x20) [ 1.840507] r8:c07db3fc r7:c07d8410 r6:c097e400 r5:00000007 r4:c08ee14c [ 1.847573] [<c07e0be8>] (am33xx_init_late+0x0/0x20) from [<c07db420>] (init_machine_late+0x24/0x30) [ 1.857173] [<c07db3fc>] (init_machine_late+0x0/0x30) from [<c00089ec>] (do_one_initcall+0xf4/0x154) [ 1.866766] [<c00088f8>] (do_one_initcall+0x0/0x154) from [<c07d8b94>] (kernel_init_freeable+0xf0/0x1bc) [ 1.876726] [<c07d8aa4>] (kernel_init_freeable+0x0/0x1bc) from [<c05cb654>] (kernel_init+0x10/0xec) [ 1.886237] [<c05cb644>] (kernel_init+0x0/0xec) from [<c00146f8>] (ret_from_fork+0x14/0x3c) [ 1.895005] r4:00000000 r3:00000000 [ 1.898795] ---[ end trace 746e089ac4a8ece1 ]---[
As pointed out here, this might be caused by the PMIC tps65910 running on i2c-1 instead of i2c-0.
But the PMIC is running well, our issue is the sleep mode.
I suppose we have some I2c misconfiguration in our DeviceTree.
According to Documentation/devicetree/bindings/i2c/i2c-omap.txt, this should be correct.
Could someone please have a look on it?
i2c1: i2c@4802a000{
pinctrl-name = "default";
pinctrl-0 =<&i2c1_pins>;
status = "okay";
clock-frequency =<400000>;
//ti,hwmods = "i2c1";
/* Set OPP50 (0.95V) for VDD core */
sleep-sequence = /bits/ 8 <
0x02 0x2d 0x25 0x1f /* Set VDD2 to 0.95V */
>;
/* Set OPP100 (1.10V) for VDD core */
wake-sequence = /bits/ 8 <
0x02 0x2d 0x25 0x2b /* Set VDD2 to 1.1V */
>;
tps: tps@2d {
reg = <0x2d>;
};
tlv320aic3x: tlv320aic3x@18 {
compatible = "ti,tlv320aic32x4"; /* ti,tlv320aic3x*/
reg = <0x18>;
status = "okay";
/* Regulators */
AVDD-supply = <&vaux2_reg>;
IOVDD-supply = <&vaux2_reg>;
DRVDD-supply = <&vaux2_reg>;
DVDD-supply = <&vbat>;
};
};
i2c2: i2c@4819c000{
pinctrl-name = "default";
pinctrl-0 =<&i2c2_pins>;
status = "okay";
clock-frequency =<400000>;
// ti,hwmods = "i2c2";
tsc:tsc@55 {
reg = <0x55>;
};
gdx:gdx@5d {
reg = <0x5d>;
};
};
Best regards,
Roland