This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Linux SDK 6.0 DeepSleep issue

Other Parts Discussed in Thread: SYSCONFIG

We are using PSP 04.06.00.11. Our 5V regulator is controlled by gpio1_8. Gpio bank 1 looses context during suspend and it isn't restored correctly on resume.  There does appear to be some context restore related functions in gpio-omap.c but they are targeted for the OMAP3 processors.


There are a series of commits that seem to have been meant to fix this but they were all reverted without any comment on why.

  • arm:omap:gpio - Handle Clocks properly in Suspend/Resume
  • Revert "arm:omap:gpio - Handle Clocks properly in Suspend/Resume"
  • gpio/omap: use flag to identify wakeup domain
  • gpio/omap: handle save/restore context in GPIO driver
  • gpio/omap: fix invalid context restore of gpio bank-0
  • gpio/omap: save and restore debounce registers
  • Revert "gpio/omap: save and restore debounce registers"
  • Revert "gpio/omap: fix invalid context restore of gpio bank-0"
  • Revert "gpio/omap: handle save/restore context in GPIO driver"
  • Revert "gpio/omap: use flag to identify wakeup domain"

Author: Hebbar, Gururaja <gururaja.hebbar@ti.com> 

Committer: Vishveshwar Bhat <vishveshwar.bhat@ti.com> 


Register differences from before sleep to after resume

GPIO1

GPIO_SYSCONFIG

-0x4804C010 - 0x0000001D
+0x4804C010 - 0x00000000

0h = Force-idle. An idle request is acknowledged unconditionally
0h = Wakeup generation is disabled.
0h = Internal Interface OCP clock is free-running

GPIO_SYSSTAT

-0x4804C114 - 0x00000001
+0x4804C114 - 0x00000000

0h = Internal Reset is on-going.

GPIO_CTRL

-0x4804C130 - 0x00000000
+0x4804C130 - 0x00000002

1h = Functional clock is interface clock divided by 2.

GPIO_OE

-0x4804C134 - 0xFE7D0EFF
+0x4804C134 - 0xFFFFFFFF

1h = The corresponding GPIO port is configured as an input.

GPIO_DATAIN

-0x4804C138 - 0x00410200
+0x4804C138 - 0x00010200

Sampled Input Data

GPIO2

-0x481AC010 - 0x0000001D
+0x481AC010 - 0x00000000
-0x481AC114 - 0x00000001
+0x481AC114 - 0x00000000
-0x481AC130 - 0x00000000
+0x481AC130 - 0x00000002
-0x481AC134 - 0xFFEFFFFF
+0x481AC134 - 0xFFFFFFFF

GPIO3

-0x481AE010 - 0x0000001D
+0x481AE010 - 0x00000000
-0x481AE114 - 0x00000001
+0x481AE114 - 0x00000000
-0x481AE130 - 0x00000000
+0x481AE130 - 0x00000002

  • I will forward this to the software team, but please be aware that PSP 04.06.00.11 is very old and no longer maintained.
  • Hi Jonathan,

    Do you use AM335x custom board? Can you reproduce this issue on AM335x TI board? Can you reproduce this issue with the latest PSDK 3.00.00.04?

    What is your wake-up source (UART0/console, GPIO0, Touchscreen)?

    In order to avoid data loss, it is recommended that the users issue a "sync" command before suspending the system.

    Make sure you are fully aligned with the below wiki pages:

    processors.wiki.ti.com/.../AM335x-PSP_04.06.00.11_Release_Notes
    processors.wiki.ti.com/.../AM335x-PSP_04.06.00.11_Features_and_Performance_Guide

    processors.wiki.ti.com/.../AM335x_Linux_Power_Management_User_Guide
    processors.wiki.ti.com/.../AM335x_Power_Management_Standby_User's_Guide

    Regards,
    Pavel
  • More to add:

    GPIO 1,2,3 are in PER Power domain which goes off during DeepSleep0 while GPIO0 is in Wakeup Power domain and is always ON. Most of our drivers do a context save and restore during Suspend/resume.

    Also /drivers/gpio/gpio-omap.c is the gpio driver and it takes care of the context save/restore for gpio, manipulation of clocks and power rails is not done here.

    You can try add code to omap_gpio_suspend() and omap_gpio_resume() in gpio-omap.c, for the case METHOD_GPIO_44XX, to save and restore the OE and the DATAOUT registers (add elements to the gpio_bank struct for the saved values) and see if the GPIOs recover to a usable state.
  • Biser Gatchev-XID said:
    I will forward this to the software team, but please be aware that PSP 04.06.00.11 is very old and no longer maintained.

    Biser, Yeah I'm aware.  Sadly the newer kernels don't work with the version of android you guys last released and have stopped supporting. Thanks.
     

  • Pavel Botev said:
    More to add:

    GPIO 1,2,3 are in PER Power domain which goes off during DeepSleep0 while GPIO0 is in Wakeup Power domain and is always ON. Most of our drivers do a context save and restore during Suspend/resume.

    Also /drivers/gpio/gpio-omap.c is the gpio driver and it takes care of the context save/restore for gpio, manipulation of clocks and power rails is not done here.

    You can try add code to omap_gpio_suspend() and omap_gpio_resume() in gpio-omap.c, for the case METHOD_GPIO_44XX, to save and restore the OE and the DATAOUT registers (add elements to the gpio_bank struct for the saved values) and see if the GPIOs recover to a usable state.

    Pavel, Thanks for the reply. That is actually what these patches do. I have recommitted (unreverted them :) ) them and the gpio context is now being restored.  I am concerned that these were reverted for a reason and there might be some bug I'm not seeing.

    • gpio/omap: use flag to identify wakeup domain
    • gpio/omap: handle save/restore context in GPIO driver
    • gpio/omap: fix invalid context restore of gpio bank-0
    • gpio/omap: save and restore debounce registers

    There have been probably >100 changes in the mainline kernel for gpio-omap.c, most of them seem targeted for restoring context and other sleep mode things.  These 4 commits were cherry-picked from there by Hebbar, Gururaja <gururaja.hebbar@ti.com>.

    arm:omap:gpio - Handle Clocks properly in Suspend/Resume
    Restoring this commit had no effect on the gpio registers or on sleep mode power usage. So I have left it reverted.

    I am using a GPIO0 pin to wake from mem sleep.

    After applying the commits however the SYSCONFIG registers are still not being restored.  I seem to be able to read and control the gpio's just fine so I'm not sure what effect this will have.  I have also not been able to find where in the kernel these registers are controlled.

    --- gpio_patch_1first.txt	2016-07-21 15:22:31.705626023 -0400
    +++ gpio_patch_4resume.txt	2016-07-21 15:24:04.317624436 -0400
    @@ -28,7 +28,7 @@
     
     GPIO1
    -0x4804C010 - 0x0000001D
    +0x4804C010 - 0x00000000
    -0x4804C114 - 0x00000001
    +0x4804C114 - 0x00000000
     
     GPIO2
    -0x481AC010 - 0x0000001D
    +0x481AC010 - 0x00000000
    -0x481AC114 - 0x00000001
    +0x481AC114 - 0x00000000
     
     GPIO3
    -0x481AE010 - 0x0000001D
    +0x481AE010 - 0x00000000
    -0x481AE114 - 0x00000001
    +0x481AE114 - 0x00000000
    

  • Pavel Botev said:
    Hi Jonathan,

    Do you use AM335x custom board? Can you reproduce this issue on AM335x TI board? Can you reproduce this issue with the latest PSDK 3.00.00.04?

    In order to avoid data loss, it is recommended that the users issue a "sync" command before suspending the system.

    Yes this is a custom board.  I have not tried to reproduce it but I see no reason it wouldn't have the same issue considering it uses the same gpio-omap.c driver.  Considering the large number of gpio-omap.c patches, I suspect this isn't an issue.

    Why would issuing sync manually be necessary?  Is there a bug with the sync that power management does?

    [  118.393249] PM: Syncing filesystems ... done.

  • Jonathan,

    Jonathan Cormier said:
    That is actually what these patches do. I have recommitted (unreverted them :) ) them and the gpio context is now being restored.  I am concerned that these were reverted for a reason and there might be some bug I'm not seeing.

    Can you provide me a link to these patches? See also the latest version of the gpio-omap.c driver (attached) taken from the latest AM335x PSDK:

    ti-processor-sdk-linux-am335x-evm-03.00.00.04/board-support/linux-4.4.12/drivers/gpio/gpio-omap.c

    /*
     * Support functions for OMAP GPIO
     *
     * Copyright (C) 2003-2005 Nokia Corporation
     * Written by Juha Yrjölä <juha.yrjola@nokia.com>
     *
     * Copyright (C) 2009 Texas Instruments
     * Added OMAP4 support - Santosh Shilimkar <santosh.shilimkar@ti.com>
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    #include <linux/init.h>
    #include <linux/module.h>
    #include <linux/interrupt.h>
    #include <linux/syscore_ops.h>
    #include <linux/err.h>
    #include <linux/clk.h>
    #include <linux/io.h>
    #include <linux/device.h>
    #include <linux/pm_runtime.h>
    #include <linux/pm.h>
    #include <linux/of.h>
    #include <linux/of_device.h>
    #include <linux/gpio.h>
    #include <linux/bitops.h>
    #include <linux/platform_data/gpio-omap.h>
    
    #define OFF_MODE	1
    #define OMAP4_GPIO_DEBOUNCINGTIME_MASK 0xFF
    
    static LIST_HEAD(omap_gpio_list);
    
    struct gpio_regs {
    	u32 irqenable1;
    	u32 irqenable2;
    	u32 wake_en;
    	u32 ctrl;
    	u32 oe;
    	u32 leveldetect0;
    	u32 leveldetect1;
    	u32 risingdetect;
    	u32 fallingdetect;
    	u32 dataout;
    	u32 debounce;
    	u32 debounce_en;
    };
    
    struct gpio_bank {
    	struct list_head node;
    	void __iomem *base;
    	int irq;
    	u32 non_wakeup_gpios;
    	u32 enabled_non_wakeup_gpios;
    	struct gpio_regs context;
    	u32 saved_datain;
    	u32 level_mask;
    	u32 toggle_mask;
    	raw_spinlock_t lock;
    	raw_spinlock_t wa_lock;
    	struct gpio_chip chip;
    	struct clk *dbck;
    	u32 mod_usage;
    	u32 irq_usage;
    	u32 dbck_enable_mask;
    	bool dbck_enabled;
    	struct device *dev;
    	bool is_mpuio;
    	bool dbck_flag;
    
    	bool context_valid;
    	int stride;
    	u32 width;
    	int context_loss_count;
    	int power_mode;
    	bool workaround_enabled;
    
    	void (*set_dataout)(struct gpio_bank *bank, unsigned gpio, int enable);
    	int (*get_context_loss_count)(struct device *dev);
    
    	struct omap_gpio_reg_offs *regs;
    };
    
    #define GPIO_MOD_CTRL_BIT	BIT(0)
    
    #define BANK_USED(bank) (bank->mod_usage || bank->irq_usage)
    #define LINE_USED(line, offset) (line & (BIT(offset)))
    
    static void omap_gpio_unmask_irq(struct irq_data *d);
    
    static inline struct gpio_bank *omap_irq_data_get_bank(struct irq_data *d)
    {
    	struct gpio_chip *chip = irq_data_get_irq_chip_data(d);
    	return container_of(chip, struct gpio_bank, chip);
    }
    
    static void omap_set_gpio_direction(struct gpio_bank *bank, int gpio,
    				    int is_input)
    {
    	void __iomem *reg = bank->base;
    	u32 l;
    
    	reg += bank->regs->direction;
    	l = readl_relaxed(reg);
    	if (is_input)
    		l |= BIT(gpio);
    	else
    		l &= ~(BIT(gpio));
    	writel_relaxed(l, reg);
    	bank->context.oe = l;
    }
    
    
    /* set data out value using dedicate set/clear register */
    static void omap_set_gpio_dataout_reg(struct gpio_bank *bank, unsigned offset,
    				      int enable)
    {
    	void __iomem *reg = bank->base;
    	u32 l = BIT(offset);
    
    	if (enable) {
    		reg += bank->regs->set_dataout;
    		bank->context.dataout |= l;
    	} else {
    		reg += bank->regs->clr_dataout;
    		bank->context.dataout &= ~l;
    	}
    
    	writel_relaxed(l, reg);
    }
    
    /* set data out value using mask register */
    static void omap_set_gpio_dataout_mask(struct gpio_bank *bank, unsigned offset,
    				       int enable)
    {
    	void __iomem *reg = bank->base + bank->regs->dataout;
    	u32 gpio_bit = BIT(offset);
    	u32 l;
    
    	l = readl_relaxed(reg);
    	if (enable)
    		l |= gpio_bit;
    	else
    		l &= ~gpio_bit;
    	writel_relaxed(l, reg);
    	bank->context.dataout = l;
    }
    
    static int omap_get_gpio_datain(struct gpio_bank *bank, int offset)
    {
    	void __iomem *reg = bank->base + bank->regs->datain;
    
    	return (readl_relaxed(reg) & (BIT(offset))) != 0;
    }
    
    static int omap_get_gpio_dataout(struct gpio_bank *bank, int offset)
    {
    	void __iomem *reg = bank->base + bank->regs->dataout;
    
    	return (readl_relaxed(reg) & (BIT(offset))) != 0;
    }
    
    static inline void omap_gpio_rmw(void __iomem *base, u32 reg, u32 mask, bool set)
    {
    	int l = readl_relaxed(base + reg);
    
    	if (set)
    		l |= mask;
    	else
    		l &= ~mask;
    
    	writel_relaxed(l, base + reg);
    }
    
    static inline void omap_gpio_dbck_enable(struct gpio_bank *bank)
    {
    	if (bank->dbck_enable_mask && !bank->dbck_enabled) {
    		clk_enable(bank->dbck);
    		bank->dbck_enabled = true;
    
    		writel_relaxed(bank->dbck_enable_mask,
    			     bank->base + bank->regs->debounce_en);
    	}
    }
    
    static inline void omap_gpio_dbck_disable(struct gpio_bank *bank)
    {
    	if (bank->dbck_enable_mask && bank->dbck_enabled) {
    		/*
    		 * Disable debounce before cutting it's clock. If debounce is
    		 * enabled but the clock is not, GPIO module seems to be unable
    		 * to detect events and generate interrupts at least on OMAP3.
    		 */
    		writel_relaxed(0, bank->base + bank->regs->debounce_en);
    
    		clk_disable(bank->dbck);
    		bank->dbck_enabled = false;
    	}
    }
    
    /**
     * omap2_set_gpio_debounce - low level gpio debounce time
     * @bank: the gpio bank we're acting upon
     * @offset: the gpio number on this @bank
     * @debounce: debounce time to use
     *
     * OMAP's debounce time is in 31us steps
     *   <debounce time> = (GPIO_DEBOUNCINGTIME[7:0].DEBOUNCETIME + 1) x 31
     * so we need to convert and round up to the closest unit.
     */
    static void omap2_set_gpio_debounce(struct gpio_bank *bank, unsigned offset,
    				    unsigned debounce)
    {
    	void __iomem		*reg;
    	u32			val;
    	u32			l;
    	bool			enable = !!debounce;
    
    	if (!bank->dbck_flag)
    		return;
    
    	if (enable) {
    		debounce = DIV_ROUND_UP(debounce, 31) - 1;
    		debounce &= OMAP4_GPIO_DEBOUNCINGTIME_MASK;
    	}
    
    	l = BIT(offset);
    
    	clk_enable(bank->dbck);
    	reg = bank->base + bank->regs->debounce;
    	writel_relaxed(debounce, reg);
    
    	reg = bank->base + bank->regs->debounce_en;
    	val = readl_relaxed(reg);
    
    	if (enable)
    		val |= l;
    	else
    		val &= ~l;
    	bank->dbck_enable_mask = val;
    
    	writel_relaxed(val, reg);
    	clk_disable(bank->dbck);
    	/*
    	 * Enable debounce clock per module.
    	 * This call is mandatory because in omap_gpio_request() when
    	 * *_runtime_get_sync() is called,  _gpio_dbck_enable() within
    	 * runtime callbck fails to turn on dbck because dbck_enable_mask
    	 * used within _gpio_dbck_enable() is still not initialized at
    	 * that point. Therefore we have to enable dbck here.
    	 */
    	omap_gpio_dbck_enable(bank);
    	if (bank->dbck_enable_mask) {
    		bank->context.debounce = debounce;
    		bank->context.debounce_en = val;
    	}
    }
    
    /**
     * omap_clear_gpio_debounce - clear debounce settings for a gpio
     * @bank: the gpio bank we're acting upon
     * @offset: the gpio number on this @bank
     *
     * If a gpio is using debounce, then clear the debounce enable bit and if
     * this is the only gpio in this bank using debounce, then clear the debounce
     * time too. The debounce clock will also be disabled when calling this function
     * if this is the only gpio in the bank using debounce.
     */
    static void omap_clear_gpio_debounce(struct gpio_bank *bank, unsigned offset)
    {
    	u32 gpio_bit = BIT(offset);
    
    	if (!bank->dbck_flag)
    		return;
    
    	if (!(bank->dbck_enable_mask & gpio_bit))
    		return;
    
    	bank->dbck_enable_mask &= ~gpio_bit;
    	bank->context.debounce_en &= ~gpio_bit;
            writel_relaxed(bank->context.debounce_en,
    		     bank->base + bank->regs->debounce_en);
    
    	if (!bank->dbck_enable_mask) {
    		bank->context.debounce = 0;
    		writel_relaxed(bank->context.debounce, bank->base +
    			     bank->regs->debounce);
    		clk_disable(bank->dbck);
    		bank->dbck_enabled = false;
    	}
    }
    
    static inline void omap_set_gpio_trigger(struct gpio_bank *bank, int gpio,
    						unsigned trigger)
    {
    	void __iomem *base = bank->base;
    	u32 gpio_bit = BIT(gpio);
    
    	omap_gpio_rmw(base, bank->regs->leveldetect0, gpio_bit,
    		      trigger & IRQ_TYPE_LEVEL_LOW);
    	omap_gpio_rmw(base, bank->regs->leveldetect1, gpio_bit,
    		      trigger & IRQ_TYPE_LEVEL_HIGH);
    	omap_gpio_rmw(base, bank->regs->risingdetect, gpio_bit,
    		      trigger & IRQ_TYPE_EDGE_RISING);
    	omap_gpio_rmw(base, bank->regs->fallingdetect, gpio_bit,
    		      trigger & IRQ_TYPE_EDGE_FALLING);
    
    	bank->context.leveldetect0 =
    			readl_relaxed(bank->base + bank->regs->leveldetect0);
    	bank->context.leveldetect1 =
    			readl_relaxed(bank->base + bank->regs->leveldetect1);
    	bank->context.risingdetect =
    			readl_relaxed(bank->base + bank->regs->risingdetect);
    	bank->context.fallingdetect =
    			readl_relaxed(bank->base + bank->regs->fallingdetect);
    
    	if (likely(!(bank->non_wakeup_gpios & gpio_bit))) {
    		omap_gpio_rmw(base, bank->regs->wkup_en, gpio_bit, trigger != 0);
    		bank->context.wake_en =
    			readl_relaxed(bank->base + bank->regs->wkup_en);
    	}
    
    	/* This part needs to be executed always for OMAP{34xx, 44xx} */
    	if (!bank->regs->irqctrl) {
    		/* On omap24xx proceed only when valid GPIO bit is set */
    		if (bank->non_wakeup_gpios) {
    			if (!(bank->non_wakeup_gpios & gpio_bit))
    				goto exit;
    		}
    
    		/*
    		 * Log the edge gpio and manually trigger the IRQ
    		 * after resume if the input level changes
    		 * to avoid irq lost during PER RET/OFF mode
    		 * Applies for omap2 non-wakeup gpio and all omap3 gpios
    		 */
    		if (trigger & IRQ_TYPE_EDGE_BOTH)
    			bank->enabled_non_wakeup_gpios |= gpio_bit;
    		else
    			bank->enabled_non_wakeup_gpios &= ~gpio_bit;
    	}
    
    exit:
    	bank->level_mask =
    		readl_relaxed(bank->base + bank->regs->leveldetect0) |
    		readl_relaxed(bank->base + bank->regs->leveldetect1);
    }
    
    #ifdef CONFIG_ARCH_OMAP1
    /*
     * This only applies to chips that can't do both rising and falling edge
     * detection at once.  For all other chips, this function is a noop.
     */
    static void omap_toggle_gpio_edge_triggering(struct gpio_bank *bank, int gpio)
    {
    	void __iomem *reg = bank->base;
    	u32 l = 0;
    
    	if (!bank->regs->irqctrl)
    		return;
    
    	reg += bank->regs->irqctrl;
    
    	l = readl_relaxed(reg);
    	if ((l >> gpio) & 1)
    		l &= ~(BIT(gpio));
    	else
    		l |= BIT(gpio);
    
    	writel_relaxed(l, reg);
    }
    #else
    static void omap_toggle_gpio_edge_triggering(struct gpio_bank *bank, int gpio) {}
    #endif
    
    static int omap_set_gpio_triggering(struct gpio_bank *bank, int gpio,
    				    unsigned trigger)
    {
    	void __iomem *reg = bank->base;
    	void __iomem *base = bank->base;
    	u32 l = 0;
    
    	if (bank->regs->leveldetect0 && bank->regs->wkup_en) {
    		omap_set_gpio_trigger(bank, gpio, trigger);
    	} else if (bank->regs->irqctrl) {
    		reg += bank->regs->irqctrl;
    
    		l = readl_relaxed(reg);
    		if ((trigger & IRQ_TYPE_SENSE_MASK) == IRQ_TYPE_EDGE_BOTH)
    			bank->toggle_mask |= BIT(gpio);
    		if (trigger & IRQ_TYPE_EDGE_RISING)
    			l |= BIT(gpio);
    		else if (trigger & IRQ_TYPE_EDGE_FALLING)
    			l &= ~(BIT(gpio));
    		else
    			return -EINVAL;
    
    		writel_relaxed(l, reg);
    	} else if (bank->regs->edgectrl1) {
    		if (gpio & 0x08)
    			reg += bank->regs->edgectrl2;
    		else
    			reg += bank->regs->edgectrl1;
    
    		gpio &= 0x07;
    		l = readl_relaxed(reg);
    		l &= ~(3 << (gpio << 1));
    		if (trigger & IRQ_TYPE_EDGE_RISING)
    			l |= 2 << (gpio << 1);
    		if (trigger & IRQ_TYPE_EDGE_FALLING)
    			l |= BIT(gpio << 1);
    
    		/* Enable wake-up during idle for dynamic tick */
    		omap_gpio_rmw(base, bank->regs->wkup_en, BIT(gpio), trigger);
    		bank->context.wake_en =
    			readl_relaxed(bank->base + bank->regs->wkup_en);
    		writel_relaxed(l, reg);
    	}
    	return 0;
    }
    
    static void omap_enable_gpio_module(struct gpio_bank *bank, unsigned offset)
    {
    	if (bank->regs->pinctrl) {
    		void __iomem *reg = bank->base + bank->regs->pinctrl;
    
    		/* Claim the pin for MPU */
    		writel_relaxed(readl_relaxed(reg) | (BIT(offset)), reg);
    	}
    
    	if (bank->regs->ctrl && !BANK_USED(bank)) {
    		void __iomem *reg = bank->base + bank->regs->ctrl;
    		u32 ctrl;
    
    		ctrl = readl_relaxed(reg);
    		/* Module is enabled, clocks are not gated */
    		ctrl &= ~GPIO_MOD_CTRL_BIT;
    		writel_relaxed(ctrl, reg);
    		bank->context.ctrl = ctrl;
    	}
    }
    
    static void omap_disable_gpio_module(struct gpio_bank *bank, unsigned offset)
    {
    	void __iomem *base = bank->base;
    
    	if (bank->regs->wkup_en &&
    	    !LINE_USED(bank->mod_usage, offset) &&
    	    !LINE_USED(bank->irq_usage, offset)) {
    		/* Disable wake-up during idle for dynamic tick */
    		omap_gpio_rmw(base, bank->regs->wkup_en, BIT(offset), 0);
    		bank->context.wake_en =
    			readl_relaxed(bank->base + bank->regs->wkup_en);
    	}
    
    	if (bank->regs->ctrl && !BANK_USED(bank)) {
    		void __iomem *reg = bank->base + bank->regs->ctrl;
    		u32 ctrl;
    
    		ctrl = readl_relaxed(reg);
    		/* Module is disabled, clocks are gated */
    		ctrl |= GPIO_MOD_CTRL_BIT;
    		writel_relaxed(ctrl, reg);
    		bank->context.ctrl = ctrl;
    	}
    }
    
    static int omap_gpio_is_input(struct gpio_bank *bank, unsigned offset)
    {
    	void __iomem *reg = bank->base + bank->regs->direction;
    
    	return readl_relaxed(reg) & BIT(offset);
    }
    
    static void omap_gpio_init_irq(struct gpio_bank *bank, unsigned offset)
    {
    	if (!LINE_USED(bank->mod_usage, offset)) {
    		omap_enable_gpio_module(bank, offset);
    		omap_set_gpio_direction(bank, offset, 1);
    	}
    	bank->irq_usage |= BIT(offset);
    }
    
    static int omap_gpio_irq_type(struct irq_data *d, unsigned type)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	int retval;
    	unsigned long flags;
    	unsigned offset = d->hwirq;
    
    	if (type & ~IRQ_TYPE_SENSE_MASK)
    		return -EINVAL;
    
    	if (!bank->regs->leveldetect0 &&
    		(type & (IRQ_TYPE_LEVEL_LOW|IRQ_TYPE_LEVEL_HIGH)))
    		return -EINVAL;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	retval = omap_set_gpio_triggering(bank, offset, type);
    	if (retval) {
    		raw_spin_unlock_irqrestore(&bank->lock, flags);
    		goto error;
    	}
    	omap_gpio_init_irq(bank, offset);
    	if (!omap_gpio_is_input(bank, offset)) {
    		raw_spin_unlock_irqrestore(&bank->lock, flags);
    		retval = -EINVAL;
    		goto error;
    	}
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	if (type & (IRQ_TYPE_LEVEL_LOW | IRQ_TYPE_LEVEL_HIGH))
    		irq_set_handler_locked(d, handle_level_irq);
    	else if (type & (IRQ_TYPE_EDGE_FALLING | IRQ_TYPE_EDGE_RISING))
    		irq_set_handler_locked(d, handle_edge_irq);
    
    	return 0;
    
    error:
    	return retval;
    }
    
    static void omap_clear_gpio_irqbank(struct gpio_bank *bank, int gpio_mask)
    {
    	void __iomem *reg = bank->base;
    
    	reg += bank->regs->irqstatus;
    	writel_relaxed(gpio_mask, reg);
    
    	/* Workaround for clearing DSP GPIO interrupts to allow retention */
    	if (bank->regs->irqstatus2) {
    		reg = bank->base + bank->regs->irqstatus2;
    		writel_relaxed(gpio_mask, reg);
    	}
    
    	/* Flush posted write for the irq status to avoid spurious interrupts */
    	readl_relaxed(reg);
    }
    
    static inline void omap_clear_gpio_irqstatus(struct gpio_bank *bank,
    					     unsigned offset)
    {
    	omap_clear_gpio_irqbank(bank, BIT(offset));
    }
    
    static u32 omap_get_gpio_irqbank_mask(struct gpio_bank *bank)
    {
    	void __iomem *reg = bank->base;
    	u32 l;
    	u32 mask = (BIT(bank->width)) - 1;
    
    	reg += bank->regs->irqenable;
    	l = readl_relaxed(reg);
    	if (bank->regs->irqenable_inv)
    		l = ~l;
    	l &= mask;
    	return l;
    }
    
    static void omap_enable_gpio_irqbank(struct gpio_bank *bank, int gpio_mask)
    {
    	void __iomem *reg = bank->base;
    	u32 l;
    
    	if (bank->regs->set_irqenable) {
    		reg += bank->regs->set_irqenable;
    		l = gpio_mask;
    		bank->context.irqenable1 |= gpio_mask;
    	} else {
    		reg += bank->regs->irqenable;
    		l = readl_relaxed(reg);
    		if (bank->regs->irqenable_inv)
    			l &= ~gpio_mask;
    		else
    			l |= gpio_mask;
    		bank->context.irqenable1 = l;
    	}
    
    	writel_relaxed(l, reg);
    }
    
    static void omap_disable_gpio_irqbank(struct gpio_bank *bank, int gpio_mask)
    {
    	void __iomem *reg = bank->base;
    	u32 l;
    
    	if (bank->regs->clr_irqenable) {
    		reg += bank->regs->clr_irqenable;
    		l = gpio_mask;
    		bank->context.irqenable1 &= ~gpio_mask;
    	} else {
    		reg += bank->regs->irqenable;
    		l = readl_relaxed(reg);
    		if (bank->regs->irqenable_inv)
    			l |= gpio_mask;
    		else
    			l &= ~gpio_mask;
    		bank->context.irqenable1 = l;
    	}
    
    	writel_relaxed(l, reg);
    }
    
    static inline void omap_set_gpio_irqenable(struct gpio_bank *bank,
    					   unsigned offset, int enable)
    {
    	if (enable)
    		omap_enable_gpio_irqbank(bank, BIT(offset));
    	else
    		omap_disable_gpio_irqbank(bank, BIT(offset));
    }
    
    /* Use disable_irq_wake() and enable_irq_wake() functions from drivers */
    static int omap_gpio_wake_enable(struct irq_data *d, unsigned int enable)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    
    	return irq_set_irq_wake(bank->irq, enable);
    }
    
    static int omap_gpio_request(struct gpio_chip *chip, unsigned offset)
    {
    	struct gpio_bank *bank = container_of(chip, struct gpio_bank, chip);
    	unsigned long flags;
    
    	/*
    	 * If this is the first gpio_request for the bank,
    	 * enable the bank module.
    	 */
    	if (!BANK_USED(bank))
    		pm_runtime_get_sync(bank->dev);
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	omap_enable_gpio_module(bank, offset);
    	bank->mod_usage |= BIT(offset);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    
    static void omap_gpio_free(struct gpio_chip *chip, unsigned offset)
    {
    	struct gpio_bank *bank = container_of(chip, struct gpio_bank, chip);
    	unsigned long flags;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	bank->mod_usage &= ~(BIT(offset));
    	if (!LINE_USED(bank->irq_usage, offset)) {
    		omap_set_gpio_direction(bank, offset, 1);
    		omap_clear_gpio_debounce(bank, offset);
    	}
    	omap_disable_gpio_module(bank, offset);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	/*
    	 * If this is the last gpio to be freed in the bank,
    	 * disable the bank module.
    	 */
    	if (!BANK_USED(bank))
    		pm_runtime_put(bank->dev);
    }
    
    /*
     * We need to unmask the GPIO bank interrupt as soon as possible to
     * avoid missing GPIO interrupts for other lines in the bank.
     * Then we need to mask-read-clear-unmask the triggered GPIO lines
     * in the bank to avoid missing nested interrupts for a GPIO line.
     * If we wait to unmask individual GPIO lines in the bank after the
     * line's interrupt handler has been run, we may miss some nested
     * interrupts.
     */
    static irqreturn_t omap_gpio_irq_handler(int irq, void *gpiobank)
    {
    	void __iomem *isr_reg = NULL;
    	u32 isr;
    	unsigned int bit;
    	struct gpio_bank *bank = gpiobank;
    	unsigned long wa_lock_flags;
    	unsigned long lock_flags;
    
    	isr_reg = bank->base + bank->regs->irqstatus;
    	if (WARN_ON(!isr_reg))
    		goto exit;
    
    	pm_runtime_get_sync(bank->dev);
    
    	while (1) {
    		u32 isr_saved, level_mask = 0;
    		u32 enabled;
    
    		raw_spin_lock_irqsave(&bank->lock, lock_flags);
    
    		enabled = omap_get_gpio_irqbank_mask(bank);
    		isr_saved = isr = readl_relaxed(isr_reg) & enabled;
    
    		if (bank->level_mask)
    			level_mask = bank->level_mask & enabled;
    
    		/* clear edge sensitive interrupts before handler(s) are
    		called so that we don't miss any interrupt occurred while
    		executing them */
    		omap_disable_gpio_irqbank(bank, isr_saved & ~level_mask);
    		omap_clear_gpio_irqbank(bank, isr_saved & ~level_mask);
    		omap_enable_gpio_irqbank(bank, isr_saved & ~level_mask);
    
    		raw_spin_unlock_irqrestore(&bank->lock, lock_flags);
    
    		if (!isr)
    			break;
    
    		while (isr) {
    			bit = __ffs(isr);
    			isr &= ~(BIT(bit));
    
    			raw_spin_lock_irqsave(&bank->lock, lock_flags);
    			/*
    			 * Some chips can't respond to both rising and falling
    			 * at the same time.  If this irq was requested with
    			 * both flags, we need to flip the ICR data for the IRQ
    			 * to respond to the IRQ for the opposite direction.
    			 * This will be indicated in the bank toggle_mask.
    			 */
    			if (bank->toggle_mask & (BIT(bit)))
    				omap_toggle_gpio_edge_triggering(bank, bit);
    
    			raw_spin_unlock_irqrestore(&bank->lock, lock_flags);
    
    			raw_spin_lock_irqsave(&bank->wa_lock, wa_lock_flags);
    
    			generic_handle_irq(irq_find_mapping(bank->chip.irqdomain,
    							    bit));
    
    			raw_spin_unlock_irqrestore(&bank->wa_lock,
    						   wa_lock_flags);
    		}
    	}
    exit:
    	pm_runtime_put(bank->dev);
    	return IRQ_HANDLED;
    }
    
    static unsigned int omap_gpio_irq_startup(struct irq_data *d)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	unsigned long flags;
    	unsigned offset = d->hwirq;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    
    	if (!LINE_USED(bank->mod_usage, offset))
    		omap_set_gpio_direction(bank, offset, 1);
    	else if (!omap_gpio_is_input(bank, offset))
    		goto err;
    	omap_enable_gpio_module(bank, offset);
    	bank->irq_usage |= BIT(offset);
    
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    	omap_gpio_unmask_irq(d);
    
    	return 0;
    err:
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    	return -EINVAL;
    }
    
    static void omap_gpio_irq_shutdown(struct irq_data *d)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	unsigned long flags;
    	unsigned offset = d->hwirq;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	bank->irq_usage &= ~(BIT(offset));
    	omap_set_gpio_irqenable(bank, offset, 0);
    	omap_clear_gpio_irqstatus(bank, offset);
    	omap_set_gpio_triggering(bank, offset, IRQ_TYPE_NONE);
    	if (!LINE_USED(bank->mod_usage, offset))
    		omap_clear_gpio_debounce(bank, offset);
    	omap_disable_gpio_module(bank, offset);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    }
    
    static void omap_gpio_irq_bus_lock(struct irq_data *data)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(data);
    
    	if (!BANK_USED(bank))
    		pm_runtime_get_sync(bank->dev);
    }
    
    static void gpio_irq_bus_sync_unlock(struct irq_data *data)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(data);
    
    	/*
    	 * If this is the last IRQ to be freed in the bank,
    	 * disable the bank module.
    	 */
    	if (!BANK_USED(bank))
    		pm_runtime_put(bank->dev);
    }
    
    static void omap_gpio_ack_irq(struct irq_data *d)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	unsigned offset = d->hwirq;
    
    	omap_clear_gpio_irqstatus(bank, offset);
    }
    
    static void omap_gpio_mask_irq(struct irq_data *d)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	unsigned offset = d->hwirq;
    	unsigned long flags;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	omap_set_gpio_irqenable(bank, offset, 0);
    	omap_set_gpio_triggering(bank, offset, IRQ_TYPE_NONE);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    }
    
    static void omap_gpio_unmask_irq(struct irq_data *d)
    {
    	struct gpio_bank *bank = omap_irq_data_get_bank(d);
    	unsigned offset = d->hwirq;
    	u32 trigger = irqd_get_trigger_type(d);
    	unsigned long flags;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	if (trigger)
    		omap_set_gpio_triggering(bank, offset, trigger);
    
    	/* For level-triggered GPIOs, the clearing must be done after
    	 * the HW source is cleared, thus after the handler has run */
    	if (bank->level_mask & BIT(offset)) {
    		omap_set_gpio_irqenable(bank, offset, 0);
    		omap_clear_gpio_irqstatus(bank, offset);
    	}
    
    	omap_set_gpio_irqenable(bank, offset, 1);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    }
    
    /*---------------------------------------------------------------------*/
    
    static int omap_mpuio_suspend_noirq(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct gpio_bank	*bank = platform_get_drvdata(pdev);
    	void __iomem		*mask_reg = bank->base +
    					OMAP_MPUIO_GPIO_MASKIT / bank->stride;
    	unsigned long		flags;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	writel_relaxed(0xffff & ~bank->context.wake_en, mask_reg);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    
    static int omap_mpuio_resume_noirq(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct gpio_bank	*bank = platform_get_drvdata(pdev);
    	void __iomem		*mask_reg = bank->base +
    					OMAP_MPUIO_GPIO_MASKIT / bank->stride;
    	unsigned long		flags;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	writel_relaxed(bank->context.wake_en, mask_reg);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    
    static const struct dev_pm_ops omap_mpuio_dev_pm_ops = {
    	.suspend_noirq = omap_mpuio_suspend_noirq,
    	.resume_noirq = omap_mpuio_resume_noirq,
    };
    
    /* use platform_driver for this. */
    static struct platform_driver omap_mpuio_driver = {
    	.driver		= {
    		.name	= "mpuio",
    		.pm	= &omap_mpuio_dev_pm_ops,
    	},
    };
    
    static struct platform_device omap_mpuio_device = {
    	.name		= "mpuio",
    	.id		= -1,
    	.dev = {
    		.driver = &omap_mpuio_driver.driver,
    	}
    	/* could list the /proc/iomem resources */
    };
    
    static inline void omap_mpuio_init(struct gpio_bank *bank)
    {
    	platform_set_drvdata(&omap_mpuio_device, bank);
    
    	if (platform_driver_register(&omap_mpuio_driver) == 0)
    		(void) platform_device_register(&omap_mpuio_device);
    }
    
    /*---------------------------------------------------------------------*/
    
    static int omap_gpio_get_direction(struct gpio_chip *chip, unsigned offset)
    {
    	struct gpio_bank *bank;
    	unsigned long flags;
    	void __iomem *reg;
    	int dir;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    	reg = bank->base + bank->regs->direction;
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	dir = !!(readl_relaxed(reg) & BIT(offset));
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    	return dir;
    }
    
    static int omap_gpio_input(struct gpio_chip *chip, unsigned offset)
    {
    	struct gpio_bank *bank;
    	unsigned long flags;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	omap_set_gpio_direction(bank, offset, 1);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    	return 0;
    }
    
    static int omap_gpio_get(struct gpio_chip *chip, unsigned offset)
    {
    	struct gpio_bank *bank;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    
    	if (omap_gpio_is_input(bank, offset))
    		return omap_get_gpio_datain(bank, offset);
    	else
    		return omap_get_gpio_dataout(bank, offset);
    }
    
    static int omap_gpio_output(struct gpio_chip *chip, unsigned offset, int value)
    {
    	struct gpio_bank *bank;
    	unsigned long flags;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	bank->set_dataout(bank, offset, value);
    	omap_set_gpio_direction(bank, offset, 0);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    	return 0;
    }
    
    static int omap_gpio_debounce(struct gpio_chip *chip, unsigned offset,
    			      unsigned debounce)
    {
    	struct gpio_bank *bank;
    	unsigned long flags;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	omap2_set_gpio_debounce(bank, offset, debounce);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    
    static void omap_gpio_set(struct gpio_chip *chip, unsigned offset, int value)
    {
    	struct gpio_bank *bank;
    	unsigned long flags;
    
    	bank = container_of(chip, struct gpio_bank, chip);
    	raw_spin_lock_irqsave(&bank->lock, flags);
    	bank->set_dataout(bank, offset, value);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    }
    
    /*---------------------------------------------------------------------*/
    
    static void __init omap_gpio_show_rev(struct gpio_bank *bank)
    {
    	static bool called;
    	u32 rev;
    
    	if (called || bank->regs->revision == USHRT_MAX)
    		return;
    
    	rev = readw_relaxed(bank->base + bank->regs->revision);
    	pr_info("OMAP GPIO hardware version %d.%d\n",
    		(rev >> 4) & 0x0f, rev & 0x0f);
    
    	called = true;
    }
    
    static void omap_gpio_mod_init(struct gpio_bank *bank)
    {
    	void __iomem *base = bank->base;
    	u32 l = 0xffffffff;
    
    	if (bank->width == 16)
    		l = 0xffff;
    
    	if (bank->is_mpuio) {
    		writel_relaxed(l, bank->base + bank->regs->irqenable);
    		return;
    	}
    
    	omap_gpio_rmw(base, bank->regs->irqenable, l,
    		      bank->regs->irqenable_inv);
    	omap_gpio_rmw(base, bank->regs->irqstatus, l,
    		      !bank->regs->irqenable_inv);
    	if (bank->regs->debounce_en)
    		writel_relaxed(0, base + bank->regs->debounce_en);
    
    	/* Save OE default value (0xffffffff) in the context */
    	bank->context.oe = readl_relaxed(bank->base + bank->regs->direction);
    	 /* Initialize interface clk ungated, module enabled */
    	if (bank->regs->ctrl)
    		writel_relaxed(0, base + bank->regs->ctrl);
    }
    
    static int omap_gpio_chip_init(struct gpio_bank *bank, struct irq_chip *irqc)
    {
    	static int gpio;
    	int irq_base = 0;
    	int ret;
    
    	/*
    	 * REVISIT eventually switch from OMAP-specific gpio structs
    	 * over to the generic ones
    	 */
    	bank->chip.request = omap_gpio_request;
    	bank->chip.free = omap_gpio_free;
    	bank->chip.get_direction = omap_gpio_get_direction;
    	bank->chip.direction_input = omap_gpio_input;
    	bank->chip.get = omap_gpio_get;
    	bank->chip.direction_output = omap_gpio_output;
    	bank->chip.set_debounce = omap_gpio_debounce;
    	bank->chip.set = omap_gpio_set;
    	if (bank->is_mpuio) {
    		bank->chip.label = "mpuio";
    		if (bank->regs->wkup_en)
    			bank->chip.dev = &omap_mpuio_device.dev;
    		bank->chip.base = OMAP_MPUIO(0);
    	} else {
    		bank->chip.label = "gpio";
    		bank->chip.base = gpio;
    	}
    	bank->chip.ngpio = bank->width;
    
    	ret = gpiochip_add(&bank->chip);
    	if (ret) {
    		dev_err(bank->dev, "Could not register gpio chip %d\n", ret);
    		return ret;
    	}
    
    	if (!bank->is_mpuio)
    		gpio += bank->width;
    
    #ifdef CONFIG_ARCH_OMAP1
    	/*
    	 * REVISIT: Once we have OMAP1 supporting SPARSE_IRQ, we can drop
    	 * irq_alloc_descs() since a base IRQ offset will no longer be needed.
    	 */
    	irq_base = irq_alloc_descs(-1, 0, bank->width, 0);
    	if (irq_base < 0) {
    		dev_err(bank->dev, "Couldn't allocate IRQ numbers\n");
    		return -ENODEV;
    	}
    #endif
    
    	/* MPUIO is a bit different, reading IRQ status clears it */
    	if (bank->is_mpuio) {
    		irqc->irq_ack = dummy_irq_chip.irq_ack;
    		if (!bank->regs->wkup_en)
    			irqc->irq_set_wake = NULL;
    	}
    
    	ret = gpiochip_irqchip_add(&bank->chip, irqc,
    				   irq_base, handle_bad_irq,
    				   IRQ_TYPE_NONE);
    
    	if (ret) {
    		dev_err(bank->dev, "Couldn't add irqchip to gpiochip %d\n", ret);
    		gpiochip_remove(&bank->chip);
    		return -ENODEV;
    	}
    
    	gpiochip_set_chained_irqchip(&bank->chip, irqc, bank->irq, NULL);
    
    	ret = devm_request_irq(bank->dev, bank->irq, omap_gpio_irq_handler,
    			       0, dev_name(bank->dev), bank);
    	if (ret)
    		gpiochip_remove(&bank->chip);
    
    	return ret;
    }
    
    static const struct of_device_id omap_gpio_match[];
    
    static int omap_gpio_probe(struct platform_device *pdev)
    {
    	struct device *dev = &pdev->dev;
    	struct device_node *node = dev->of_node;
    	const struct of_device_id *match;
    	const struct omap_gpio_platform_data *pdata;
    	struct resource *res;
    	struct gpio_bank *bank;
    	struct irq_chip *irqc;
    	int ret;
    
    	match = of_match_device(of_match_ptr(omap_gpio_match), dev);
    
    	pdata = match ? match->data : dev_get_platdata(dev);
    	if (!pdata)
    		return -EINVAL;
    
    	bank = devm_kzalloc(dev, sizeof(struct gpio_bank), GFP_KERNEL);
    	if (!bank) {
    		dev_err(dev, "Memory alloc failed\n");
    		return -ENOMEM;
    	}
    
    	irqc = devm_kzalloc(dev, sizeof(*irqc), GFP_KERNEL);
    	if (!irqc)
    		return -ENOMEM;
    
    	irqc->irq_startup = omap_gpio_irq_startup,
    	irqc->irq_shutdown = omap_gpio_irq_shutdown,
    	irqc->irq_ack = omap_gpio_ack_irq,
    	irqc->irq_mask = omap_gpio_mask_irq,
    	irqc->irq_unmask = omap_gpio_unmask_irq,
    	irqc->irq_set_type = omap_gpio_irq_type,
    	irqc->irq_set_wake = omap_gpio_wake_enable,
    	irqc->irq_bus_lock = omap_gpio_irq_bus_lock,
    	irqc->irq_bus_sync_unlock = gpio_irq_bus_sync_unlock,
    	irqc->name = dev_name(&pdev->dev);
    	irqc->flags = IRQCHIP_MASK_ON_SUSPEND;
    
    	bank->irq = platform_get_irq(pdev, 0);
    	if (bank->irq <= 0) {
    		if (!bank->irq)
    			bank->irq = -ENXIO;
    		if (bank->irq != -EPROBE_DEFER)
    			dev_err(dev,
    				"can't get irq resource ret=%d\n", bank->irq);
    		return bank->irq;
    	}
    
    	bank->dev = dev;
    	bank->chip.dev = dev;
    	bank->chip.owner = THIS_MODULE;
    	bank->dbck_flag = pdata->dbck_flag;
    	bank->stride = pdata->bank_stride;
    	bank->width = pdata->bank_width;
    	bank->is_mpuio = pdata->is_mpuio;
    	bank->non_wakeup_gpios = pdata->non_wakeup_gpios;
    	bank->regs = pdata->regs;
    #ifdef CONFIG_OF_GPIO
    	bank->chip.of_node = of_node_get(node);
    #endif
    	if (!node) {
    		bank->get_context_loss_count =
    			pdata->get_context_loss_count;
    	}
    
    	if (bank->regs->set_dataout && bank->regs->clr_dataout)
    		bank->set_dataout = omap_set_gpio_dataout_reg;
    	else
    		bank->set_dataout = omap_set_gpio_dataout_mask;
    
    	raw_spin_lock_init(&bank->lock);
    	raw_spin_lock_init(&bank->wa_lock);
    
    	/* Static mapping, never released */
    	res = platform_get_resource(pdev, IORESOURCE_MEM, 0);
    	bank->base = devm_ioremap_resource(dev, res);
    	if (IS_ERR(bank->base)) {
    		return PTR_ERR(bank->base);
    	}
    
    	if (bank->dbck_flag) {
    		bank->dbck = devm_clk_get(bank->dev, "dbclk");
    		if (IS_ERR(bank->dbck)) {
    			dev_err(bank->dev,
    				"Could not get gpio dbck. Disable debounce\n");
    			bank->dbck_flag = false;
    		} else {
    			clk_prepare(bank->dbck);
    		}
    	}
    
    	platform_set_drvdata(pdev, bank);
    
    	pm_runtime_enable(bank->dev);
    	pm_runtime_irq_safe(bank->dev);
    	pm_runtime_get_sync(bank->dev);
    
    	if (bank->is_mpuio)
    		omap_mpuio_init(bank);
    
    	omap_gpio_mod_init(bank);
    
    	ret = omap_gpio_chip_init(bank, irqc);
    	if (ret) {
    		pm_runtime_put_sync(bank->dev);
    		pm_runtime_disable(bank->dev);
    		return ret;
    	}
    
    	omap_gpio_show_rev(bank);
    
    	pm_runtime_put(bank->dev);
    
    	list_add_tail(&bank->node, &omap_gpio_list);
    
    	return 0;
    }
    
    static int omap_gpio_remove(struct platform_device *pdev)
    {
    	struct gpio_bank *bank = platform_get_drvdata(pdev);
    
    	list_del(&bank->node);
    	gpiochip_remove(&bank->chip);
    	pm_runtime_disable(bank->dev);
    	if (bank->dbck_flag)
    		clk_unprepare(bank->dbck);
    
    	return 0;
    }
    
    #ifdef CONFIG_ARCH_OMAP2PLUS
    
    #if defined(CONFIG_PM)
    static void omap_gpio_restore_context(struct gpio_bank *bank);
    
    static int omap_gpio_runtime_suspend(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct gpio_bank *bank = platform_get_drvdata(pdev);
    	u32 l1 = 0, l2 = 0;
    	unsigned long flags;
    	u32 wake_low, wake_hi;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    
    	/*
    	 * Only edges can generate a wakeup event to the PRCM.
    	 *
    	 * Therefore, ensure any wake-up capable GPIOs have
    	 * edge-detection enabled before going idle to ensure a wakeup
    	 * to the PRCM is generated on a GPIO transition. (c.f. 34xx
    	 * NDA TRM 25.5.3.1)
    	 *
    	 * The normal values will be restored upon ->runtime_resume()
    	 * by writing back the values saved in bank->context.
    	 */
    	wake_low = bank->context.leveldetect0 & bank->context.wake_en;
    	if (wake_low)
    		writel_relaxed(wake_low | bank->context.fallingdetect,
    			     bank->base + bank->regs->fallingdetect);
    	wake_hi = bank->context.leveldetect1 & bank->context.wake_en;
    	if (wake_hi)
    		writel_relaxed(wake_hi | bank->context.risingdetect,
    			     bank->base + bank->regs->risingdetect);
    
    	if (!bank->enabled_non_wakeup_gpios)
    		goto update_gpio_context_count;
    
    	if (bank->power_mode != OFF_MODE) {
    		bank->power_mode = 0;
    		goto update_gpio_context_count;
    	}
    	/*
    	 * If going to OFF, remove triggering for all
    	 * non-wakeup GPIOs.  Otherwise spurious IRQs will be
    	 * generated.  See OMAP2420 Errata item 1.101.
    	 */
    	bank->saved_datain = readl_relaxed(bank->base +
    						bank->regs->datain);
    	l1 = bank->context.fallingdetect;
    	l2 = bank->context.risingdetect;
    
    	l1 &= ~bank->enabled_non_wakeup_gpios;
    	l2 &= ~bank->enabled_non_wakeup_gpios;
    
    	writel_relaxed(l1, bank->base + bank->regs->fallingdetect);
    	writel_relaxed(l2, bank->base + bank->regs->risingdetect);
    
    	bank->workaround_enabled = true;
    
    update_gpio_context_count:
    	if (bank->get_context_loss_count)
    		bank->context_loss_count =
    				bank->get_context_loss_count(bank->dev);
    
    	omap_gpio_dbck_disable(bank);
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    
    static void omap_gpio_init_context(struct gpio_bank *p);
    
    static int omap_gpio_runtime_resume(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct gpio_bank *bank = platform_get_drvdata(pdev);
    	u32 l = 0, gen, gen0, gen1;
    	unsigned long flags;
    	int c;
    
    	raw_spin_lock_irqsave(&bank->lock, flags);
    
    	/*
    	 * On the first resume during the probe, the context has not
    	 * been initialised and so initialise it now. Also initialise
    	 * the context loss count.
    	 */
    	if (!bank->context_valid) {
    		omap_gpio_init_context(bank);
    
    		if (bank->get_context_loss_count)
    			bank->context_loss_count =
    				bank->get_context_loss_count(bank->dev);
    	}
    
    	omap_gpio_dbck_enable(bank);
    
    	/*
    	 * In ->runtime_suspend(), level-triggered, wakeup-enabled
    	 * GPIOs were set to edge trigger also in order to be able to
    	 * generate a PRCM wakeup.  Here we restore the
    	 * pre-runtime_suspend() values for edge triggering.
    	 */
    	writel_relaxed(bank->context.fallingdetect,
    		     bank->base + bank->regs->fallingdetect);
    	writel_relaxed(bank->context.risingdetect,
    		     bank->base + bank->regs->risingdetect);
    
    	if (!bank->get_context_loss_count) {
    		omap_gpio_restore_context(bank);
    	} else {
    		c = bank->get_context_loss_count(bank->dev);
    		if (c != bank->context_loss_count) {
    			raw_spin_unlock_irqrestore(&bank->lock, flags);
    			return 0;
    		}
    	}
    
    	if (!bank->workaround_enabled) {
    		raw_spin_unlock_irqrestore(&bank->lock, flags);
    		return 0;
    	}
    
    	l = readl_relaxed(bank->base + bank->regs->datain);
    
    	/*
    	 * Check if any of the non-wakeup interrupt GPIOs have changed
    	 * state.  If so, generate an IRQ by software.  This is
    	 * horribly racy, but it's the best we can do to work around
    	 * this silicon bug.
    	 */
    	l ^= bank->saved_datain;
    	l &= bank->enabled_non_wakeup_gpios;
    
    	/*
    	 * No need to generate IRQs for the rising edge for gpio IRQs
    	 * configured with falling edge only; and vice versa.
    	 */
    	gen0 = l & bank->context.fallingdetect;
    	gen0 &= bank->saved_datain;
    
    	gen1 = l & bank->context.risingdetect;
    	gen1 &= ~(bank->saved_datain);
    
    	/* FIXME: Consider GPIO IRQs with level detections properly! */
    	gen = l & (~(bank->context.fallingdetect) &
    					 ~(bank->context.risingdetect));
    	/* Consider all GPIO IRQs needed to be updated */
    	gen |= gen0 | gen1;
    
    	if (gen) {
    		u32 old0, old1;
    
    		old0 = readl_relaxed(bank->base + bank->regs->leveldetect0);
    		old1 = readl_relaxed(bank->base + bank->regs->leveldetect1);
    
    		if (!bank->regs->irqstatus_raw0) {
    			writel_relaxed(old0 | gen, bank->base +
    						bank->regs->leveldetect0);
    			writel_relaxed(old1 | gen, bank->base +
    						bank->regs->leveldetect1);
    		}
    
    		if (bank->regs->irqstatus_raw0) {
    			writel_relaxed(old0 | l, bank->base +
    						bank->regs->leveldetect0);
    			writel_relaxed(old1 | l, bank->base +
    						bank->regs->leveldetect1);
    		}
    		writel_relaxed(old0, bank->base + bank->regs->leveldetect0);
    		writel_relaxed(old1, bank->base + bank->regs->leveldetect1);
    	}
    
    	bank->workaround_enabled = false;
    	raw_spin_unlock_irqrestore(&bank->lock, flags);
    
    	return 0;
    }
    #endif /* CONFIG_PM */
    
    #if IS_BUILTIN(CONFIG_GPIO_OMAP)
    void omap2_gpio_prepare_for_idle(int pwr_mode)
    {
    	struct gpio_bank *bank;
    
    	list_for_each_entry(bank, &omap_gpio_list, node) {
    		if (!BANK_USED(bank))
    			continue;
    
    		bank->power_mode = pwr_mode;
    
    		pm_runtime_put_sync_suspend(bank->dev);
    	}
    }
    
    void omap2_gpio_resume_after_idle(void)
    {
    	struct gpio_bank *bank;
    
    	list_for_each_entry(bank, &omap_gpio_list, node) {
    		if (!BANK_USED(bank))
    			continue;
    
    		pm_runtime_get_sync(bank->dev);
    	}
    }
    #endif
    
    #if defined(CONFIG_PM)
    static void omap_gpio_init_context(struct gpio_bank *p)
    {
    	struct omap_gpio_reg_offs *regs = p->regs;
    	void __iomem *base = p->base;
    
    	p->context.ctrl		= readl_relaxed(base + regs->ctrl);
    	p->context.oe		= readl_relaxed(base + regs->direction);
    	p->context.wake_en	= readl_relaxed(base + regs->wkup_en);
    	p->context.leveldetect0	= readl_relaxed(base + regs->leveldetect0);
    	p->context.leveldetect1	= readl_relaxed(base + regs->leveldetect1);
    	p->context.risingdetect	= readl_relaxed(base + regs->risingdetect);
    	p->context.fallingdetect = readl_relaxed(base + regs->fallingdetect);
    	p->context.irqenable1	= readl_relaxed(base + regs->irqenable);
    	p->context.irqenable2	= readl_relaxed(base + regs->irqenable2);
    
    	if (regs->set_dataout && p->regs->clr_dataout)
    		p->context.dataout = readl_relaxed(base + regs->set_dataout);
    	else
    		p->context.dataout = readl_relaxed(base + regs->dataout);
    
    	p->context_valid = true;
    }
    
    static void omap_gpio_restore_context(struct gpio_bank *bank)
    {
    	writel_relaxed(bank->context.wake_en,
    				bank->base + bank->regs->wkup_en);
    	writel_relaxed(bank->context.ctrl, bank->base + bank->regs->ctrl);
    	writel_relaxed(bank->context.leveldetect0,
    				bank->base + bank->regs->leveldetect0);
    	writel_relaxed(bank->context.leveldetect1,
    				bank->base + bank->regs->leveldetect1);
    	writel_relaxed(bank->context.risingdetect,
    				bank->base + bank->regs->risingdetect);
    	writel_relaxed(bank->context.fallingdetect,
    				bank->base + bank->regs->fallingdetect);
    	if (bank->regs->set_dataout && bank->regs->clr_dataout)
    		writel_relaxed(bank->context.dataout,
    				bank->base + bank->regs->set_dataout);
    	else
    		writel_relaxed(bank->context.dataout,
    				bank->base + bank->regs->dataout);
    	writel_relaxed(bank->context.oe, bank->base + bank->regs->direction);
    
    	if (bank->dbck_enable_mask) {
    		writel_relaxed(bank->context.debounce, bank->base +
    					bank->regs->debounce);
    		writel_relaxed(bank->context.debounce_en,
    					bank->base + bank->regs->debounce_en);
    	}
    
    	writel_relaxed(bank->context.irqenable1,
    				bank->base + bank->regs->irqenable);
    	writel_relaxed(bank->context.irqenable2,
    				bank->base + bank->regs->irqenable2);
    }
    #endif /* CONFIG_PM */
    #else
    #define omap_gpio_runtime_suspend NULL
    #define omap_gpio_runtime_resume NULL
    static inline void omap_gpio_init_context(struct gpio_bank *p) {}
    #endif
    
    static const struct dev_pm_ops gpio_pm_ops = {
    	SET_RUNTIME_PM_OPS(omap_gpio_runtime_suspend, omap_gpio_runtime_resume,
    									NULL)
    };
    
    #if defined(CONFIG_OF)
    static struct omap_gpio_reg_offs omap2_gpio_regs = {
    	.revision =		OMAP24XX_GPIO_REVISION,
    	.direction =		OMAP24XX_GPIO_OE,
    	.datain =		OMAP24XX_GPIO_DATAIN,
    	.dataout =		OMAP24XX_GPIO_DATAOUT,
    	.set_dataout =		OMAP24XX_GPIO_SETDATAOUT,
    	.clr_dataout =		OMAP24XX_GPIO_CLEARDATAOUT,
    	.irqstatus =		OMAP24XX_GPIO_IRQSTATUS1,
    	.irqstatus2 =		OMAP24XX_GPIO_IRQSTATUS2,
    	.irqenable =		OMAP24XX_GPIO_IRQENABLE1,
    	.irqenable2 =		OMAP24XX_GPIO_IRQENABLE2,
    	.set_irqenable =	OMAP24XX_GPIO_SETIRQENABLE1,
    	.clr_irqenable =	OMAP24XX_GPIO_CLEARIRQENABLE1,
    	.debounce =		OMAP24XX_GPIO_DEBOUNCE_VAL,
    	.debounce_en =		OMAP24XX_GPIO_DEBOUNCE_EN,
    	.ctrl =			OMAP24XX_GPIO_CTRL,
    	.wkup_en =		OMAP24XX_GPIO_WAKE_EN,
    	.leveldetect0 =		OMAP24XX_GPIO_LEVELDETECT0,
    	.leveldetect1 =		OMAP24XX_GPIO_LEVELDETECT1,
    	.risingdetect =		OMAP24XX_GPIO_RISINGDETECT,
    	.fallingdetect =	OMAP24XX_GPIO_FALLINGDETECT,
    };
    
    static struct omap_gpio_reg_offs omap4_gpio_regs = {
    	.revision =		OMAP4_GPIO_REVISION,
    	.direction =		OMAP4_GPIO_OE,
    	.datain =		OMAP4_GPIO_DATAIN,
    	.dataout =		OMAP4_GPIO_DATAOUT,
    	.set_dataout =		OMAP4_GPIO_SETDATAOUT,
    	.clr_dataout =		OMAP4_GPIO_CLEARDATAOUT,
    	.irqstatus =		OMAP4_GPIO_IRQSTATUS0,
    	.irqstatus2 =		OMAP4_GPIO_IRQSTATUS1,
    	.irqenable =		OMAP4_GPIO_IRQSTATUSSET0,
    	.irqenable2 =		OMAP4_GPIO_IRQSTATUSSET1,
    	.set_irqenable =	OMAP4_GPIO_IRQSTATUSSET0,
    	.clr_irqenable =	OMAP4_GPIO_IRQSTATUSCLR0,
    	.debounce =		OMAP4_GPIO_DEBOUNCINGTIME,
    	.debounce_en =		OMAP4_GPIO_DEBOUNCENABLE,
    	.ctrl =			OMAP4_GPIO_CTRL,
    	.wkup_en =		OMAP4_GPIO_IRQWAKEN0,
    	.leveldetect0 =		OMAP4_GPIO_LEVELDETECT0,
    	.leveldetect1 =		OMAP4_GPIO_LEVELDETECT1,
    	.risingdetect =		OMAP4_GPIO_RISINGDETECT,
    	.fallingdetect =	OMAP4_GPIO_FALLINGDETECT,
    };
    
    static const struct omap_gpio_platform_data omap2_pdata = {
    	.regs = &omap2_gpio_regs,
    	.bank_width = 32,
    	.dbck_flag = false,
    };
    
    static const struct omap_gpio_platform_data omap3_pdata = {
    	.regs = &omap2_gpio_regs,
    	.bank_width = 32,
    	.dbck_flag = true,
    };
    
    static const struct omap_gpio_platform_data omap4_pdata = {
    	.regs = &omap4_gpio_regs,
    	.bank_width = 32,
    	.dbck_flag = true,
    };
    
    static const struct of_device_id omap_gpio_match[] = {
    	{
    		.compatible = "ti,omap4-gpio",
    		.data = &omap4_pdata,
    	},
    	{
    		.compatible = "ti,omap3-gpio",
    		.data = &omap3_pdata,
    	},
    	{
    		.compatible = "ti,omap2-gpio",
    		.data = &omap2_pdata,
    	},
    	{ },
    };
    MODULE_DEVICE_TABLE(of, omap_gpio_match);
    #endif
    
    static struct platform_driver omap_gpio_driver = {
    	.probe		= omap_gpio_probe,
    	.remove		= omap_gpio_remove,
    	.driver		= {
    		.name	= "omap_gpio",
    		.pm	= &gpio_pm_ops,
    		.of_match_table = of_match_ptr(omap_gpio_match),
    	},
    };
    
    /*
     * gpio driver register needs to be done before
     * machine_init functions access gpio APIs.
     * Hence omap_gpio_drv_reg() is a postcore_initcall.
     */
    static int __init omap_gpio_drv_reg(void)
    {
    	return platform_driver_register(&omap_gpio_driver);
    }
    postcore_initcall(omap_gpio_drv_reg);
    
    static void __exit omap_gpio_exit(void)
    {
    	platform_driver_unregister(&omap_gpio_driver);
    }
    module_exit(omap_gpio_exit);
    
    MODULE_DESCRIPTION("omap gpio driver");
    MODULE_ALIAS("platform:gpio-omap");
    MODULE_LICENSE("GPL v2");
    

    Regards,
    Pavel

  • Jonathan Cormier said:
    Why would issuing sync manually be necessary?  Is there a bug with the sync that power management does?

    This is coming from the below wiki page:

    Regards,
    Pavel

  • Jonathan Cormier said:
    After applying the commits however the SYSCONFIG registers are still not being restored.

    I can see that sysconfig registers are not defined nor in gpio_regs neither in omap4_gpio_regs structures (linux-4.4.12/drivers/gpio/gpio-omap.c). In general you do not need this register to be saved and restored, but if you need it, you can update the registers structures adding it.

    Jonathan Cormier said:
    I have also not been able to find where in the kernel these registers are controlled.

    These GPIO registers are save and restored during suspend/resume from the below functions:

    omap_gpio_runtime_suspend()

    omap_gpio_runtime_resume()

    See also if the below wiki page will be in help, it has some info for SDK6:

    Regards,
    Pavel

  • Pavel Botev said:

    Jonathan,

    Jonathan Cormier
    That is actually what these patches do. I have recommitted (unreverted them :) ) them and the gpio context is now being restored.  I am concerned that these were reverted for a reason and there might be some bug I'm not seeing.

    Can you provide me a link to these patches? See also the latest version of the gpio-omap.c driver (attached) taken from the latest AM335x PSDK:

    ti-processor-sdk-linux-am335x-evm-03.00.00.04/board-support/linux-4.4.12/drivers/gpio/gpio-omap.c

    (Please visit the site to view this file)

    Regards,
    Pavel


    The patches can be found at the top of the following git histories:

    From arago:

    From TI: git.ti.com/.../gpio-omap.c

  • Pavel Botev said:
    Jonathan Cormier
    Why would issuing sync manually be necessary?  Is there a bug with the sync that power management does?

    This is coming from the below wiki page:

    AM335x Linux Power Management User Guide - Texas Instruments Wiki

    processors.wiki.ti.com

    Regards,
    Pavel

    Hmm I'm not sure how I would get Android to issue a sync before it suspends.

    Pavel Botev said:

    I can see that sysconfig registers are not defined nor in gpio_regs neither in omap4_gpio_regs structures (linux-4.4.12/drivers/gpio/gpio-omap.c). In general you do not need this register to be saved and restored, but if you need it, you can update the registers structures adding it.

    Alright, I haven't found any problems with them not being set so I guess its fine.

  • Jonathan Cormier said:
    arm:omap:gpio - Handle Clocks properly in Suspend/Resume
    Restoring this commit had no effect on the gpio registers or on sleep mode power usage. So I have left it reverted.

    Yes, I think you should left this patch reverted. This patch do not exist nor in the latest TI kernel v4.4.12 gpio-omap.c neither in the mainline linux v4.6 gpio-omap.c

    This patch is used to enable/disable the GPIOs functional clock (fclk) during suspend-resume. But this is now handled outside of the gpio-omap.c file. The GPIO1 fclk is controlled by CM_PER_GPIO1_CLKCTRL/0x44E000AC register. The enable/disable for this clock during suspend-resume is handled by omap_hwmod_idle() function. Refer to the below files and e2e thread for more info:


    arch/arm/mach-omap2/cm3xx.h
    arch/arm/mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c
    arch/arm/mach-omap2/omap_hwmod.c
    arch/arm/mach-omap2/omap_device.c

    I will further check regarding the other patches.

    BR
    Pavel

  • Jonathan Cormier said:
    gpio/omap: use flag to identify wakeup domain

    Taking for example this patch, I see that in the latest TI kernel v4.4.12 gpio-omap.c driver, enhanced context valid/lost technique is used, we have there:

    struct gpio_bank {

    struct gpio_regs context;

    bool context_valid;

    int context_loss_count;

    int (*get_context_loss_count)(struct device *dev);

    }

    I can not guarantee that everything will work fine in your old gpio-omap.c file, I would recommend you to align with the latest gpio-omap.c file, you should track all the changes between SDK6 and PSDK3.00.00.04 regarding gpio-omap.c.

    Regards,
    Pavel

  • Jonathan Cormier said:
    • gpio/omap: save and restore debounce registers
    • Revert "gpio/omap: save and restore debounce registers"

    AM33xx GPIO driver is compatible with omap4, and omap3_gpio_regs structure is entirely removed from the gpmc-omap.c. Debounce registers are filled up in the gpio_regs and omap4_gpio_regs structures.