Other Parts Discussed in Thread: TMS320C5515, TMS320VC5505
Hi All,
I am using the C5515 board along with CCS 4.1, from the evaluation disk shipped along with the kit.I have performed a complete installation of the software in the CD, but i dont see a DDK (Driver Development Kit) in the installation.I have created and started using a DSP/BIOS project.
My application needs an interrupt based UART driver with DMA and flow control enabled.
The DSP/BIOS Driver Developer's Guide(spru616.pdf) section 1.2.1 Functional Device Drivers, specifies that, the DDK offers complete device drivers, including the UART driver.
Should the DDK be separately downloaded/ installed ? If yes, where to find the correct version for CCS 4.1 ?
If anybody knows, please help.
Thanks in advance.
Regards
Ullas R