This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configure RESETOUT pin to GPIO on C6748



Hi all,

I want to configure RESETOUT pin to GPIO as default setting. Because the purpose is want to do PINMUX to add more delay time when initialize CMOS sensor. The hardware connection is RESETOUT to RESET of CMOS sensor. I did not add buffer IC between DSP and CMOS. Sometimes, the CMOS sesnor would occur reset failed situation. The summarized queries are as below.

1.  Add more delay time on RESETOUT pin

     Must add buffer IC instead of PINMUX switch?

2. Configure RESETOUT to GPIO in default

     Any boot issue when change PINMUX from RESETOUT to GPIO after POR?

Thanks in advance.

B.R.

OC