We have a TMS320DM6467 EVM board that was supplied with DVSDK 1.40.
I would like to work with DVSDK 2.00 on this board.
I built the DVSDK 2.00 with the following steps:
make clobber
make everything
make install
Which installed the dvsdk demos to my nfs opt shared folder.
When I attempt to run the encode/decode demos with a 720P input they fail:
Error: Failed to create capture device, 720P component input connected?
Running with CE_DEBUG=2 results in the following output:
@1,576,568us: [+2 T:0x413c8490] ti.sdo.dmai - [Capture] COMPONENT input selected
@1,576,766us: [+2 T:0x413c8490] ti.sdo.dmai - [Capture] Capture input set to COMPONENT
@1,576,965us: [+2 T:0x413c8490] ti.sdo.dmai - [Capture] Video input connected size 1920x1080 pitch 1920
@1,577,201us: [+7 T:0x413c8490] ti.sdo.dmai - [Dmai] Supplied buffers not largeenough for video standard
@1,577,331us: [+7 T:0x413c8490] ti.sdo.dmai - [Capture] Failed to intialize capture driver buffers on /dev/video0
It doesn't matter what video input I supply. It always detects 1920x1080.
Anybody come across this problem before?
Thanks,
Matt
[EDIT] Is it possible to download the Montavista Tools 5.0.0 and 4.0.1 anywhere?