This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM572x VOUT3 issue

Expert 1385 points

Other Parts Discussed in Thread: AM5728

Hi,

My customization board is based on AM5728, and my LCD use the VOUT3. But it doesn't work!  No pixel clock signal and any LCD signal from AM5728 soc.  If I use the VOUT1, everything is OK.

 I am sure that pinmux is OK, and devicetree  configuration is also ok.

and my device tree configure is as follow:

aliases {
		display0 = &lcd0;
	};
lcd0: display {
		compatible = "osddisplays,osd070t1718-19ts", "panel-dpi";

		label = "lcd";

		/* enable-gpios = <&gpio2 5 GPIO_ACTIVE_HIGH>;*/

		panel-timing {
			clock-frequency = <33000000>;
			hactive = <1024>;
			vactive = <768>;
			hfront-porch = <32>;
			hback-porch = <228>;
			hsync-len = <60>;
			vback-porch = <21>;
			vfront-porch = <7>;
			vsync-len = <10>;
			hsync-active = <0>;
			vsync-active = <0>;
			de-active = <1>;
			pixelclk-active = <1>;
		};

		port {
			lcd_in: endpoint {
				remote-endpoint = <&dpi_out>;
			};
		};
	};

&dss {
	ports {
		#address-cells = <1>;
		#size-cells = <0>;

		port {
			reg = <2>;

			dpi_out: endpoint {
				remote-endpoint = <&lcd_in>;
				data-lines = <24>;
			};
		};
	};
};

I have seen this new about VOUT2 is not support by cunnrently linux 4.13 driver.

I have traced this dss kernel code, and found this port(VOUT3) is always not enabled!  and panel_dpi_probe() has create the correct dpi panel and fb0 has been generated in system directory.

a normal DPI port is always enabled by panel_dpi_enable() in $(kernel)/drivers/video/fbdev/omap2/displays-new/panel-dpi.c,

But If I set the port:reg=2, the panel_dpi_enable() is nerver called.

 

And what I should do? can you give me some valuable suggestion?

 

 

Thank you very much!

Best Regards

Qing