This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sitara McASP internal loopback

Does anyone have an example of an internal loopback for the McASP on the AM533x or AM57x?  I have a beaglebone and was using the mcasp driver included with the starterware sdk to manipulate the registers and have yet to successfully get it to work.  I wanted to start out with the internal loopback without the signals going to the IO pads then after successful implementation add the IO pads and a jumper wire.  I am looking just to write a byte and read a byte in polling mode do demonstrate functionality and start working with the peripheral.  

So far I am 

- Turning on the clocks

- Reset TX/RX

- Configure Loopback mode

- Set RMOD and XMOD fields

- Start the transmit clock

- write to the TX Buffer

- Read the TX status register and I receive an error 0x10C

The error indicates that it is a clock error, any example would be very helpful.

Thank You,

George