This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Nitro power sequencing

Hello Team,

Can you clarify the power sequence for Nitro mode on the AM335x series (to run at 1GHz)? Specifically, since the VDD_CORE and VDD_MCU voltages need to be different, do they still ramp simultaneously or is there a desired order?

Thank You,

Casey 

  • Hi,

    No, there is no specific sequence to ramp up VDD_CORE and VDD_MCU voltages. If the recommended PMICs are used, they will start with both voltages at 1.1V and then software will boost VDD_MCU voltage for Nitro mode. If other power solution is used VDD_MCU voltage can be directly ramped up to Nitro mode voltage.