Hello,
I'd like to use DDR3 memory as 666MHz(1333). Could you tell me that a frequency of EMIF_DLL_FCLK set 333MHz is applicable or not? The max frequency of EMIF_DLL_FCLK is 266MHz.(< 333MHz) I guess a description of datasheet(SPRS957A) or a gel is typo. SYSCLK1 and DDR_DPLL_CLK are 20MHz.
I saw a dpll_ddr_config function in gel file. (CCSv6.1.2)
C:\ti\ccsv6\ccs_base\emulation\boards\am571x\gel\AM571x_prcm_config.gel
dpll_ddr_config(uint32_t DDR_FREQ)
{
uint32_t dpll_m, dpll_n, divm2, divh11, freq;
freq = DDR_FREQ;
if (666 == DDR_FREQ)
{
dpll_m = 333;
dpll_n = 4;
divm2 = 2;
divh11 = 8;
}
else if (600 == DDR_FREQ)
{
.....
}
The one of the parameters is setting for 666MHz. I input these values to CCT as below. I got 333MHz for EMIF_DLL_GCLK. EMIF_DLL_GCLK and EMIF_DLL_FCLK are connected. So EMIF_DLL_FCLK is set 333MHz. Could you give me some advice?
Regards,
Kazu